Last updated: 2014-11-28
|
Function |
Sets/queries the desired cell power level when the cell power state is on for the CW or TDSCdma system type. The optional [:SELected] keyword in this command specifies that the cell power level being set or queried applies to the current system type (TDSCdma or CW). |
|
Setting |
Range:
Resolution:0.01/1.28MHz |
|
Query |
Same as setting |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:CELL:POWER:AMPLITUDE:CW -30" |
|
Function |
The setting form of this command performs two functions: (1)sets the desired cell power level (see CALL[:CELL]:POWer:AMPLitude[:SELected])and (2)turns the cell power on/off state (see CALL[:CELL]:POWer:STATe[:SELected]) to on. The optional [:SELected] keyword in this command specifies that the cell power level being set or queried applies to the current system type (TDSCdma or CW). |
|
Setting |
Range:
Resolution:0.01/1.28MHz Note,the actual power range is defined by adding the value of the associated amplitude offset to the range |
|
Query |
Range:+37dBm/1.28MHz to -165dBm/1.28MHz or No Results Available |
|
*RST Setting |
|
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:CELL:POWER:SAMPLITUDE -30" |
|
Function |
Sets/queries the cell power state. The optional [:SELected] keyword in this command specifies that the cell power level being set or queried applies to the current system type (TDSCdma or CW). |
|
Setting |
Range:1|ON|0|OFF |
|
Query |
Range:1|0 |
|
*RST Setting |
ON |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:POWer:STATe ON" |