Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Queries the desired total RF power for the current operating mode. The total RF power is a calculated value, which is the sum of cell power and AWGN power. |
|
Query |
Range:+39.12dBm/1.28MHz to -165dBm/1.28MHz or 9.91 E+37 (NAN) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TOTal:POWer?" |
|
Function |
Queries the desired total RF power when in the TD-SCDMA Test operating mode. The total RF power is a calculated value, which is the sum of cell power and AWGN power. |
|
Query |
Range:+39.12dBm/1.28MHz to -165dBm/1.28MHz or 9.91 E+37 (NAN) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TOTal:POWer:TDSCdma?" |
|
Function |
Queries the total RF power state for the current operating mode. Note,the total RF power state is on if either cell power or AWGN power is on,and the return value for this query is not necessarily the total power state at the moment this command is processed by the test set. |
|
Query |
Range:1|0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TOTal:POWer:STATe?" |
|
Function |
Queries the total RF power state when in the TD-SCDMA Test operating mode. Note,the total RF power state is on if either cell power or AWGN power is on,and the return value for this query is not necessarily the total power state at the moment this command is processed by the test set. |
|
Query |
Range:1|0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"CALL:TOTal:POWer:STATe:TDSCdma?" |