Last updated: 2014-11-28
For more information on the GPIB Command conventions, see GPIB Command conventions
|
Function |
Sets/queries the test set's GPIB address. |
|
Setting |
Range: 0 to 30 |
|
Query |
Range: 0 to 30 |
|
*RST Setting |
14 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:GPIB:SELF:ADDRess 14" |
|
Function |
Sets/queries the test set's SCPI debugger state. When the state is on; enhanced error messages (generated from GPIB commands with syntax errors) are shown the test set display. The error message is printed along with the syntax. <ERR> is displayed at the end of the incorrect node. Non-printable characters will be replaced with the $ symbol. See Troubleshooting for a list of the errors. The debugger state should be set to on only during GPIB code development. Test times will increase if the debugger state is left on. |
|
Setting |
Range: 0|OFF | 1|ON |
|
Query |
0|1 |
|
*RST Setting |
0 (off) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTEM:COMMUNICATE:GPIB:DEBUG:STATE ON" |
|
Function |
Sets/queries the test set's LAN IP address supported in IP version 4. The LAN IP address cannot be changed when the operating mode is set to Active Cell. |
|
Setting |
Range:15 characters formatted as A.B.C.D, where A= 0 to 126 and 128 to 223, B.C.D = 0 to 255 (no embedded spaces) or blank field |
|
Query |
Range:15 characters formatted as "A.B.C.D" |
|
*RST Setting |
blank field |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:SELF:ADDRess '146.208.235.165'" |
|
Function |
Queries the LAN IPv6 Address (IID) showed in the Instrument IP Addressing screen. |
|
Query |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. |
|
*RST Setting |
Fixed value "0230:D3FF:FE02:8F58". |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:ADDRess:IP6:IID?" |
|
Function |
Sets/queries the test set's IPv6 address prefix. |
|
Query |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers.
Double-colon "::" can be used in the IPv6 address as valid. Moreover, "::" can be suffixed at the end of the 19 characters which is also a valid IPv6 address prefix. For example: 2009:1:2:3 and 2009:1:2:3:: are all valid IPv6 address prefixes for the GPIB parameter setting. |
|
Query |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. |
|
*RST Setting |
"" (Null) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:8960:8960:8960'" "SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3'" "SYSTem:COMMunicate:LAN:ADDRess:IP6:PREFix '2009:1:2:3::'" |
|
Function |
Sets/queries the test set's LAN IP address supported in IP version 4. The LAN IP address cannot be changed when the operating mode is set to Active Cell. |
|
Setting |
Range:15 characters formatted as A.B.C.D, where A= 0 to 126 and 128 to 223, B.C.D = 0 to 255 (no embedded spaces) or blank field |
|
Query |
Range:15 characters formatted as "A.B.C.D" |
|
*RST Setting |
blank field |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:SELF:ADDRess2 '146.208.235.165'" |
|
Function |
Queries the LAN 2 IPv6 Address (IID) showed in the Instrument IP Addressing screen. |
|
Query |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. |
|
*RST Setting |
Fixed value "0230:D3FF:FE02:BE5A" |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:ADDRess2:IP6:IID?" |
|
Function |
Sets/queries the LAN IP router/gateway address for the test set in IP version 4. |
|
Setting |
Range: 15 characters formatted as A.B.C.D, where A= 0 to 126 and 128 to 223, B.C.D = 0 to 255 (no embedded spaces) or blank field |
|
Query |
Range: 15 characters formatted as "A.B.C.D" |
|
*RST Setting |
blank field |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:SELF:DGATeway '255.2.6.200'" |
|
Function |
Sets/queries the test set's IPv6 Default Router Interface ID. |
|
Setting |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers.
Double-colon "::" can be used in the IPv6 Default Router Interface ID as valid. Moreover, "::" can be prefixed at the beginning of the 19 characters which is also a valid IPv6 Default Router Interface ID. For example: 8960::1, ::1:2 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. The IPv6 Default Router Interface parameter is also IPv4 address-compatible with the format: ::W.X.Y.Z, where W.X.Y.Z is the dotted decimal representation of an IPv4 address. For example, ::8960:8960:146.208.232:220 and 8960:8960:146.208.232:220 are all valid IPv6 Default Router Interface IDs for the GPIB parameter setting. |
|
Query |
Range: 19 characters formatted as: AAAA:BBBB:CCCC:DDDD where A, B, C and D are all hex numbers ranging from 0 to F. |
|
*RST Setting |
"" (Null) |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:DGATeway:IP6:IID '0000:0000:821D:B001'" |
|
Function |
Sets/queries the subnet mask of the test set based on the LAN IP address selected in IP version 4. |
|
Setting |
Range: 15 characters formatted as A.B.C.D, where A, B, C, D are between = 0 to 255 or blank field. |
|
Query |
Range: 15 characters formatted as follows: A.B.C.D where A,B,C,D are between = 0 to 255 (no embedded spaces) |
|
*RST Setting |
0.0.0.0 |
|
Requirements |
Test Application Revision: A.01.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:SELF:SMASk '255.255.0.0'" |
|
Function |
Sets/queries the external Evolved Packet Core (EPC) simulator's IPv4 address. See Ext EPC IP Addr. |
|
Setting |
Range:
|
|
Query |
Same as setting |
|
*RST Setting |
"0.0.0.0" (Null) |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:EPCore:ADDRess '130.015.156.235'" !Sets the external Evolved Packet Core (EPC) simulator's IPv4 address to '130.015.156.235'. |
|
Function |
Initiates the Connect to External EPC immediate action. See Connect To External EPC. |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:EPCore:CONNect" !Initiates a connection to the External EPC simulator. |
|
Function |
Initiates the Disconnect From External EPC immediate action. See Disconnect From External EPC. |
|
Requirements |
Test Application Revision: A.08.00 and above |
|
Programming Example |
"SYSTem:COMMunicate:LAN:EPCore:DCONnect" !Disconnect the test set from the External EPC simulator. |