SYSTem:DATE

Last updated: 2014-11-28

For more information on the GPIB Command conventions, see GPIB Command conventions

SYSTem:DATE

Function

Sets/queries the date.

Setting

Range:

  • <year> 2000 to 2099

  • <month> 1 to 12 (the number 1 corresponds to January)

  • <day> 1 to the number of days in the month specified by the <month> parameter

Query

Range: "<year>,<month>,<day>"

*RST Setting

This feature is not affected by instrument preset

Requirements

Test Application Revision: A.01.00 and above

Programming Example

"SYSTem:DATE 2009,11,11"