Last updated: January 15, 2009
The help mode implemented in your test set provides context sensitive GPIB command syntax assistance. When you put the test set into help mode, the test set displays the GPIB command syntax necessary to perform an action remotely for each action you perform from the front panel.
For example, if you put the test set into help mode and then select the test set's GPIB address, the GPIB command syntax for changing it remotely appears in the bottom left hand corner of the test set's screen.
The Help annunciator should now be displayed in the bottom of the screen.
Frequency
(
F3
). The GPIB command syntax to perform this action remotely appears in the bottom left of the screen.
Refer to the user documentation on each command for more information.