Last updated: January 15, 2009
Block Error Ratio 
measurement. 
Block Error Setup 
(
F1
) and set the measurement parameters as needed.
 Used for Data
 and 
UE Loopback Type
 to
 Type 2
.
 Close Menu 
(
F6
).
 RB Test Mode 
connection between the UE and test set (see 
How Do I Set Up a Call and Make a Connection?
).
 Trigger Arm 
is set to
 Single
, you must press the
 START SINGLE 
key to begin the measurement.
The time for the measurement to complete increases linearly with the
 Number of Blocks to Test
. For example, to test 500 blocks while on a 12.2k RMC takes approximately 10 seconds (500 blocks x 20 ms/block = 10 seconds). A measurement result is not displayed until the
 Number of Blocks to Test 
has been tested. If you are testing more than 500 blocks, the block counter increments every 500 blocks to indicate measurement progress.
Cell Power
 (
F7
),
 AWGN Power 
(
F4
),
 Soft Handover 
(
F3
) and
 Cell 2 Power 
(
F2
) as desired.An example measurement result is shown below:
For an example of performing BLER measurements while on a faded channel, refer to the:
E5515C Fading Solution Application Guide
It can be downloaded at http://cp.literature.keysight.com/litweb/pdf/1000-1894.pdf .