Last updated: January 15, 2009
Call Control 2 of 5
menu.
Cell Parameters
(
F2
).
Cell Info
(
F2
), then
Cell Parameters
(
F2
).
Auto
, if desired, so that the UE will be notified of any changes to the BCCH information transmitted by the test set after the call is established.
Set
, if required for your UE to register with the test set.
On
, if desired, to help ensure your UE will respond to the test set's page.
Close Menu
(
F6
).
Operating Mode
(
F1
) is set to
Cell Off
.
Call Control 2 of 5
menu.
Uplink Parameters
(
F4
).
Close Menu
(
F6
).
Operating Mode
(
F1
) to
Cell Off
.
Channel (UARFCN) Parms
(
F12
) and set the downlink and uplink channels to frequencies supported by your UE. Select
Return
(
F12
).
Call Parms
menus and set other call parameters as needed.
Operating Mode
(
F1
) to
Active Cell
.
UE Information
such as
IMSI
and
IMEI
on the
Call Setup
screen and the
MM Status
should change from
None
to
IMSI Attached
.
Paging Service
(
F9
) and set as needed.
Paging Service
is set to
RB Test Mode
, select
Channel Type
(
F8
) and set as needed.
Originate Call
(
F3
).
Paging Service
is set to
AMR Voice
, and
Calling Party Number Inclusion
is set to
Include
, the
Calling Party Number
is displayed on the UE's screen (see
How Do I Perform Calling Party Number Verification?
).
Connected
is displayed in the
Active Cell
window.
Connected
is displayed in the
Active Cell
window.
UE Information
.
This section is only applicable to the lab application or feature-licensed test application.
Before establishing an HSDPA connection, you may need to first set some of the parameters described in Set Cell Parameters , Set Uplink Parameters and Set Call Parameters .
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
FRC Type
to an H-Set supported by your UE or configure the user defined RB test mode channel as desired.
CN Domain
as needed. Note, before you can establish a connection in the PS domain, the UE must have attached to the test set. To enable this, the
PS Domain Information
parameter must have been set to
Present
when the UE registered with the test set. Note that
PS Domain Information
is set to
Absent
by default in the Test Application (it is set to
Present
by default in the Lab Application).
Uplink 64k DTCH for HSDPA Loopback State
as needed for your UE.
HSDPA RB Test Mode Setup
parameters as needed, then select
Close Menu
(
F6
).
MAC-hs Parameters
(
F10
),
HSDPA Uplink Parameters
(
F11
) and
H-RNTI Parameters
(
F11
on
HSDPA Parms 2 of 2
) as needed, then select
Return
(
F12
).
Absent
, the UE registers in the CS domain and
MM Status
changes from
None
to
IMSI Attached
. If
PS Domain Information
is set to
Present
, the UE should register in the CS domain and then also will register in the PS domain if it supports PS services (which causes
GMM State
to change from
None
to
Attached
).
Ensure that the
CN Domain
parameter is set to
CS Domain
if the UE did not attach to the GMM (see
Set HSDPA Parameters
).
Paging Service
(
F9
) to
RB Test Mode
.
Channel Type
(
F8
) to
12.2k RMC + HSDPA
.
Originate Call
(
F3
).
Connected
is displayed in the
Active Cell
window.
This section is only applicable to the lab application or feature-licensed test application.
Before establishing an HSPA connection, you may need to first set some of the parameters described in Set Cell Parameters , Set Uplink Parameters and Set Call Parameters .
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
FRC Type
to an H-Set supported by your UE or configure the user defined RB test mode channel as desired.
CN Domain
setting does not apply to HSPA connections (HSPA connections are always established in the PS Domain). However, before you can establish a connection in the PS domain, the UE must have attached to the test set. To enable this, the
PS Domain Information
parameter must have been set to
Present
when the UE registered with the test set. Note that
PS Domain Information
is set to
Absent
by default in the Test Application (it is set to
Present
by default in the Lab Application).
HSDPA RB Test Mode Setup
parameters as needed, then select
Close Menu
(
F6
).
MAC-hs Parameters
(
F10
),
HSDPA Uplink Parameters
(
F11
) and
H-RNTI Parameters
(
F11
on
HSDPA Parms 2 of 2
) as needed, then select
Return
(
F12
).
HSUPA Parameters
(
HSPA Parameters
(
F10
),
F9
).
HSUPA RB Test Mode Setup
(
F8
).
RB Test Mode E-DPDCH Max Channel Codes
as needed (to achieve 2 Mbps in the uplink this must be set to
2SF2
).
E-DCH RLC SDU Size
as needed (to achieve 2 Mbps in the uplink this must be set to at least
11744
).
HSUPA RB Test Mode Setup
parameters as needed, then select
Close Menu
(
F6
).
Common HSUPA Parameters
(
F9
),
Serving Grant
parameters (
F11
) and
E-RNTI Parameters
(
F11
on
HSUPA Parms 2 of 2
) as needed, then select
Return
(
F12
).
Present
, the UE should register in the CS domain (
MM Status
) and then also will register in the PS domain if it supports PS services (which causes
GMM State
to change from
None
to
Attached
).
Paging Service
(
F9
) to
RB Test Mode
.
Channel Type
(
F8
) to
12.2k RMC + HSPA
.
Originate Call
(
F3
).
Connected
is displayed in the
Active Cell
window and observe the HSUPA and HSDPA counters.
Establishing a Connection with the UE
Troubleshooting Call Processing Operations
How Do I Change Cell Parameters?
How Do I Change Uplink Parameters?