Last updated: January 15, 2009
 Operating Mode 
(
F1
) to
 Cell Off
.
 DL Channel 
(
F10
) and
 Uplink Channel 
(
F11
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
 DL Channel 
=
 10563 
and
 Uplink Channel 
=
 9613
).
 Operating Mode 
to
 Active Cell
.
 RB Test Mode 
connection between the UE and test set (see 
How Do I Set Up a Call and Make a Connection?
).
 Connected DL Channel Levels 
are set to their default values, as required by 3GPP TS 34.121 Table E.3.1 (select
 Generator Info
, 
F3 
on
 Call Control 2 of 5
).
 Cell Power 
(
F7
) to
 -93 dBm
.
 UE Target Power
:
 UL CL Power Ctrl Parameters 
(
F8
 on the
 Call Parms 3 of 3 
menu) and set
 UL CL Power Ctrl Mode 
to
 Active bits
.
 UE Target Power 
(
F7
) to the specified maximum output power for your UE (for example, 21 dBm for power class 4).The test set then drives the UE to the specified level, while also appropriately ranging its measurement receiver.
 UL CL Power Ctrl Parameters 
menu (
F8
) and set
 UL CL Power Ctrl Mode 
to
 All Up bits 
and set
 UL CL Power Ctrl Algorithm 
to
 Two
. The test set then drives the UE to transmit at the highest level possible.
 Thermal Power
. 
 Thermal Power Setup 
(F1) and set
 Trigger Arm 
to
 Single
. Select
 Close Menu 
(
F6
).