How Do I Perform Calling Party Number Verification?

How Do I Perform Calling Party Number Verification?

Last updated: January 15, 2009

This section is only applicable to the lab application.

Procedure

  1. Press the Call Setup key.
  2. Press the left More key to move to the Call Control menu 4 of 5.
  3. Press Calling Party Number Parms ( F5 ). The Calling Party Number Parameters menu is displayed. See Parameter Descriptions for details.
  4. Select Calling Party Number Inclusion .
    • Turn the knob and select Include from the drop down menu.
  5. If required, select the Calling Party Number and enter a desired value.
    • Up to 20 characters from the set of 0123456789abc*# can be entered in the entry box. The digits of 0-9 are entered from the DATA ENTRY keys and the characters of "abc*#" are entered from the newly displayed softkeys on the right of the screen.
      Enter the value in the Calling Party Number text entry

      Once the entry box goes away, the Calling Party Number field can display up to 14 characters. If the length of the entered string is greater than 14 characters, only the first 11 characters followed by a "..." are displayed in the Calling Party Number field. Use the GPIB command ( CALL:CPNumber[:SELected] ) to query the whole string.

  6. If required, select other parameters and set them to the desired value. In this example, the default settings are used.
  7. Press the Close Menu ( F6 ).
  8. (Optional) To capture a protocol log for further analysis, start a capture in the Wireless Protocol Advisor (WPA) software (see Protocol Logging ) and then perform the following steps.
  9. Set up the Call Control and Call Parms as needed for the UE to camp to the test set. Power the UE on and wait for it to camp to the test set.
  10. Verify that Paging Service ( F9 ) is set to AMR Voice for this example.
  11. Press Originate Call ( F3). The test set originates a call to the UE.
  12. Observe the UE's screen. Verify that the mobile station receives and displays the calling party number. If the Calling Party Number is not displayed on the mobile station' screen, ensure that Presentation Indicator is set to "Allowed". Answer the call on the UE, if desired.
  13. Stop WPA.
  14. If you start a WPA capture in step 5, verify that the test set sends an SETUP message with the calling party number parameters. An example log file is shown as below.

Related Topics


Calling Party Number Parameters