Last updated: January 15, 2009
|
Sets/queries the ASCII representation of the calling party number. The value is included in the SETUP message to the called mobile station when INCLude is selected by CALL:CPNumber:INCLusion . It is displayed on the called mobile station's screen when "ALLowed" is selected by CALL:CPNumber:PRESentation[:INDicator] . |
|
|
Range: 0 to 20 characters enclosed by quotes, each character from the set of 0123456789abc*# |
|
|
Range: 0 to 20 characters enclosed by quotes, each character from the set of 0123456789abc*# |
|
| Lab Application Revision: C.01 and above | |
OUTPUT 714;"CALL:CPNumber '#0123456789*'" !Sets the calling party number to #0123456789*. |
|
|
Sets/queries whether to include the calling party number information record. The value is not included in the message to the called mobile station. When "INCLude" is selected, the calling party number parameters configured by CALL:CPNumber[:SELected] , CALL:CPNumber:PLAN , CALL:CPNumber:PRESentation[:INDicator] , CALL:CPNumber:SCReening[:INDicator] and CALL:CPNumber:TYPE is sent to the mobile station. |
|
| Lab Application Revision: C.01 and above | |
OUTPUT 714;"CALL:CPNumber:INCLusion INCLude" !Set to include the calling party number to the called mobile station. |
|
|
Sets/queries the numbering plan used for the calling party number. See Parameter Descriptions for details. The value is included in the SETUP message to the called mobile station when INCLude is selected by CALL:CPNumber:INCLusion . |
|
OUTPUT 714;"CALL:CPNumber:PLAN PRIVate" !Set the numbering plan for calling party number to private. |
|
|
Sets/queries the presentation indicator (PI) used for the calling party number. See Parameter Descriptions for details. The value is included in the SETUP message to the called mobile station when INCLude is selected by CALL:CPNumber:INCLusion . |
|
OUTPUT 714;"CALL:CPNumber:PRESentation RESTricted" !Set the presentation indicator of Calling Party Number to restricted. |
|
|
Sets/queries the screening indicator (SI) for the calling party number. See Parameter Descriptions for details. The value is included in the SETUP message to the called mobile station when INCLude is selected by CALL:CPNumber:INCLusion . |
|
| Lab Application Revision: C.01 and above | |
OUTPUT 714;"CALL:CPNumber:SCReening NETWork" !Set the screening indicator of calling party number to network. |
|
|
Sets/queries the number type of the calling party number. See Parameter Descriptions for details. The value is included in the SETUP message to the called mobile station when INCLude is selected by CALL:CPNumber:INCLusion . |
|
OUTPUT 714;"CALL:CPNumber:TYPE NATional" !Set the number type of calling party number to national. |
|