How Do I Change HSUPA Parameters?

How Do I Change HSUPA Parameters?

Last updated: January 15, 2009

This section is only applicable to the lab application or feature-licensed test application.

  1. Press CALL SETUP .
  2. Select HSPA Parameters ( F10 ).
  3. Select HSUPA Parameters ( F9 ).
  4. Select HSUPA PS Data Setup ( F7 ) (lab application only) , HSUPA RB Test Mode Setup ( F8 ), Common HSUPA Parameters ( F9 ) Serving Grant ( F10 ), E-TFCI Recording ( F11 ) or E-RNTI Parameters ( F11 under HSUPA Parms 2 of 2 ).
  5. Turn the knob to highlight a parameter as desired, then press the knob to select the parameter.
  6. Enter a value or selection and press the knob.
  7. Select Close Menu ( F6 ).
  8. Select Return ( F12 ).

Related Topics


HSUPA Parameters