Last updated: January 15, 2009
|
This command determines whether all markers are turned on or turned off. |
|
| Setting | |
| *RST Setting | OFF |
OUTPUT 714;"CALCulate:SMONitor:MARKer:ALL:STATe 1" !Turns on all markers. |
|
|
This query returns the amplitude for marker <n>, where <n> is a number 1 through 3. When no marker number is specified, marker 1 is used. If you are using delta marker mode, the result is the delta marker amplitude result. (See CALCulate:SMONitor:MARKer[<n>] :MODE .) |
|
OUTPUT 714;"CALCulate:SMONitor:MARKer2:AMPLitude?" !Returns the amplitude of marker 2. |
|
|
This command sets/queries the frequency of marker <n>. where <n> is a number 1 through 3. When no marker number is specified, marker 1 is used. If you are using delta marker mode, this command sets/queries the offset frequency of the delta marker. (See CALCulate:SMONitor:MARKer[<n>] :MODE .) |
|
| Query |
|
OUTPUT 714;"CALCulate:SMONitor:MARKer:FREQuency?" !Queries the frequency of marker 1. |
|
|
This command sets/queries the time at marker <n>. where <n> is a number 1 through 3. When no marker number is specified, marker 1 is used. If you are using delta marker mode, this command sets/queries the delta offset time. (See CALCulate:SMONitor:MARKer[<n>] :MODE .) |
|
| Setting | |
| *RST Setting | 5 ms |
OUTPUT 714;"CALCulate:SMONitor:MARKer2:TIME 30" !Places marker 2 at 30 ms. |
|