Last updated: January 15, 2009
|
The setting form of this command performs two functions: (1) sets the additive white gaussian noise (AWGN) level and (2) turns the AWGN on/off state to on. The query form returns the desired AWGN power level. (See Cell Power and AWGN Power for more information about desired versus current power levels.) |
|
|
Range: -165 dBm/3.84 MHz to +35 dBm/3.84 MHz (this is the range of settings accepted, see Cell Power, AWGN Power and Total RF Power Ranges for the actual hardware range of the source). |
|
| See CALL:AWGNoise[:INTernal]:POWer:AMPLitude[:SELected] and CALL:AWGNoise[:INTernal]:POWer:STATe[:SELected] . | |
OUTPUT 714;"CALL:AWGNoise:POWer -80" ! Sets the AWGN power level to -80 dBM/3.84 MHz and turns the state on. |
|
|
Sets/queries the desired additive white gaussian noise (AWGN) level. (See Cell Power and AWGN Power for more information about desired versus current power levels.) |
|
|
Range: -165 dBm/3.84 MHz to +35 dBm/3.84 MHz, NAN (this is the range of settings accepted, see Cell Power, AWGN Power and Total RF Power Ranges for the actual hardware range of the source). |
|
| -75 dBm/3.84 MHz | |
OUTPUT 714;"CALL:AWGNoise:POWer:AMPLitude -80" ! Set the AWGN level to -80 dBM/3.84 MHz. |
|
|
Sets/queries the additive white gaussian noise (AWGN) state. |
|
OUTPUT 714;"CALL:AWGNoise:POWer:STATe ON" !Turns on AWGN. |
|