Last updated: October 19, 2012
This section is only applicable to the lab application.
|
Sets/queries the CTCH Allocation Period . This setting can not be changed in active cell operating mode (use cell off operating mode). |
|
|
The maximum number of radio frames this parameter can accept is 4096 minus the CBS Frame Offset . The command to set the CBS Frame Offset is CALL[:CELL[1]]:CTCHannel:FOFFset . |
|
| Same as setting. | |
OUTPUT 714;"CALL:CTCHannel:APERiod 50" ! Sets the CTCH Allocation Period to 50. |
|
|
Sets/queries the CBS Frame Offset . This setting can not be changed in active cell operating mode (use cell off operating mode). |
|
|
The maximum value for this command is one less than the setting for the CTCH Allocation Period . The command to set the CTCH Allocation Period is CALL[:CELL[1]]:CTCHannel:APERiod . |
|
| Same as setting. | |
OUTPUT 714;"CALL:CTCHannel:FOFFset 7" ! Sets the CBS Frame Offset to 7. |
|
|
Sets/queries the CBS Minimum Schedule Period .
This setting cannot be changed while in |
|
| Same as setting. | |
OUTPUT 714;"CALL:CTCHannel:MSPeriod 5" ! Sets the Cell Broadcast Minimum Schdule Period (number of CTCH block sets) reserved for the chedule message to 5. |
|