CALL:DAINterface
Last updated: January 15, 2009
This topic is only applicable to the lab application.
GPIB Command Conventions
CALL:DAINterface:PLAY:STARt
|
Function |
Commands the test set to start playing the digital audio file. |
|
Requirements
|
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:PLAY:STARt" !Command the test set to start playing the digital audio file.
|
CALL:DAINterface:PLAY:STATus?
|
Function |
This command queries the playing status of the digital audio file in the test set.
|
|
Query
|
Range: IDLE|READ|PLAY|DONE
|
|
Requirements |
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:PLAY:STATus?" Query the playing status of the digital audio file.
|
CALL:DAINterface:PLAY:STOP
|
Function |
Commands the test set to stop playing the digital audio file. |
|
Requirements
|
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:PLAY:STOP" !Command the test set to stop playing the digital audio file.
|
CALL:DAINterface:RECord:STARt
|
Function |
Commands the test set to start recording the digital audio file. |
|
Requirements
|
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:RECord:STARt" !Command the test set to start recording the digital audio file.
|
CALL:DAINterface:RECord:STATus?
|
Function |
This command queries the recording status of the digital audio file in the test set.
|
|
Query
|
Range: IDLE|REC|DONE
|
|
Requirements |
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:RECord:STATus?" Query the recording status of the digital audio file.
|
CALL:DAINterface:RECord:STOP
|
Function |
Commands the test set to stop recording the digital audio file. |
|
Requirements
|
Revision: E.00.16 and above
|
|
Programming Example
OUTPUT 714;"CALL:DAINterface:RECord:STOP" !Command the test set to stop recording the digital audio file.
|