CALL:OPERating

 Last updated: January 15, 2009

 GPIB Command Conventions

 CALL[:CELL]:OPERating:MODE

 Function

 Sets/queries the operating mode of the base station emulator. If a call is in progress during a change in operating mode it will be dropped.

 Setting

Range:
Active Cell Mode = CALL, UTRA FDD Test Mode = FDDTest, CW Mode = CW, Cell Off Mode = OFF

 Query

 Range: CALL|CW|FDDT|OFF

 *RST Setting

CALL

 Requirements

 Test or Lab Application Revision: A.01 and above

 Programming Example

 
OUTPUT 714;"CALL:CELL:OPERATING:MODE FDDTEST" !Selects UTRA FDD test mode.