|
Sets/queries the CS Paging Identity Type . |
|
| Same as setting | |
| IMSI | |
| Requirements | |
OUTPUT 714;"CALL:PAGing:IDENtity TMSI" ! Sets the CS Paging Identity Type to TMSI. |
|
|
Sets/queries the Number of Paging Indicators .
This parameter can only be set when |
|
| Same as setting | |
| IND18 | |
| Requirements | |
OUTPUT 714;"CALL:PAGing:INDicator:NUMBer IND36" ! Sets the number of paging indicators per frame to 36. |
|
|
Sets/queries the paging international mobile subscriber identity (IMSI). See Paging IMSI . Paging IMSI will be overwritten by the mobile station's reported IMSI during a location update or call setup. |
|
|
Range: 000000 to 9999999999999999 |
|
|
Range: "000000" to "9999999999999999" |
|
| "001012345678901" | |
| Requirements | |
OUTPUT 714;"CALL:PAGing:IMSI '023389832394287'" |
|
|
Sets/queries Repeat Paging .
This parameter can only be set when operating mode is |
|
| Range: 0|ON|1|OFF | |
| 0 (off) | |
| Requirements | |
OUTPUT 714;"CALL:PAGING:REPEAT ON" |
|
|
Sets/queries the Paging Service . |
|
| RBT | |
| Requirements |
Test Application Revision: A.04 and above. |
OUTPUT 714;"CALL:PAGing:SERVice AMR" ! Sets the paging service type to AMR voice. |
|