Last updated: November 1, 2010
|
Initiates a Reset UE Positioning Stored Information procedure. |
|
OUTPUT 714;"CALL:PPRocedure:GPSystem:MS:RESet" !Initiates a Reset UE Positioning Stored Information procedure. |
|
|
Queriesthe PCT External Control Connection State. This query returns the state of the PCT external control connection. |
|
| Range: 1|ON|0|OFF | |
| 0 | |
OUTPUT 714;"CALL:PPRocedure:PCTest:EXTernal:CTRL:STATe?" |
|
|
Sets/queries RRC Pipe State . This command also clears the measurement identity list, and resets the <sequence number> field used in the CALL:PPRocedure:RRC:PIPE:MCMessage:RESPonse[:DATA]? query to zero. |
|
| Range: 1|0 | |
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE 0" !Sets the RRC Pipe state to Off. |
|
|
Sets/queries the length (in bits) and the contents of the Assistance Data Delivery Message . If the Assistance Data Delivery Message is received while CALL:PPRocedure:RRC:PIPE[:STATe] is set to On and an RRC connection is present, the test set adds the appropriate message type parameter and integrity information if applicable, and sends the resulting message to the UE. Otherwise the message is ignored. |
|
|
Range: <length of encoded message in bits>, <"ascii string of hex digits defining message"> |
|
|
Range: <length of encoded message in bits>, <"ascii string of hex digits defining message"> |
|
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:ADDMessage?" !Queries the Assistance Data Delivery Message. |
|
|
Sets/queries the measurement identity, length (in bits), and the contents of the Measurement Control Message . If the Measurement Control Message is received while CALL:PPRocedure:RRC:PIPE[:STATe] is set to On and an RRC connection is present, the test set adds the appropriate message type parameter and integrity information if applicable. The resulting message is sent to the UE. Otherwise the message is ignored. The hex string should begin with the bit immediately following the Message Type field. That is, it should not contain the Integrity or Message type fields, as these are added by the test set. For more details on using the RRC Pipe, see RRC Pipe . |
|
|
Range: <measurement identity>, <length of encoded message in bits>, <"ascii string of hex digits defining message"> |
|
|
Range: <measurement identity>, <length of encoded message in bits>, <"ascii string of hex digits defining message"> |
|
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:MCMessage?" !Queries the Measurement Control Message. |
|
|
Queries Measurement Control Message (MCM) Response . This query returns a single message, but the last 10 messages have been stored. Messages are returned using a FIFO method. Once a message is queried, it is deleted from the memory buffer. Note that if more than 10 messages are received and none have been queried, the oldest messages are deleted to make room for the latest messages. The only Measurement Report messages that are made available over GPIB are those that appear to be associated with a Measurement Control Message that was previously originated over the RRC pipe. The application makes this determination based on the "Measurement Identity" field in the Measurement Report message. A list is maintained of all <measurement identity> messages that have been specified in any CALL:PPRocedure:RRC:PIPE:MCMessage[:DATA] commands received since the RRC pipe was enabled. When a Measurement Report message is received, the application checks the <measurement identity> field of the message and only makes it available if the identity appears in the list. |
|
|
Range: <length of encoded message in bits>, <sequence number>, <"ascii string of hex digits defining message"> |
|
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:MCMessage:RESPonse?" !Queries the MCM Response. |
|
|
Performs a Measurement Control Message (MCM) Response Clear . |
|
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:MCMessage:RESPonse:CLEar" !Performs an MCM Response Clear event. |
|
| Query |
Range: <length of encoded message in bits>, <"ascii string of hex digits defining message"> |
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:UEPosition:CAPability?" !Queries UE Positioning Capability. |
|
| Query | |
OUTPUT 714;"CALL:PPRocedure:RRC:PIPE:TSTamp:DOWNlink?" !Queries Downlink Measurement Control Message Timestamps. |
|