CALL:RBSetup

Last updated: February 20, 2014

GPIB Command Conventions

CALL[:CELL]:RBSetup:CFNHandling

Function

Sets/queries the RB Setup Timing Indication (CFN Handling) .

Setting

Range: INITialise|MAINtain

Query

Range: INIT|MAIN

*RST Setting

MAIN

Requirements

Test Application Revision: A.07 and above

Lab Application Revision: C.02 and above

Programming Example

 
OUTPUT 714;"CALL:RBSetup:CFNHandling INITialise" 
! Sets RB Setup Timing Indication (CFN Handling) to Initialise.

CALL[:CELL]:RBSetup:RLC:CONFigure

Function

Sets/queries the Radio Bearer Setup Message RLC Configuration.

This setting controls the underlying RLC configuration of the Radio Bearer Setup message sent in the DL when PS domain radio bearers are set up.This setting can not be changed in Active Cell operating mode. This setting is remote control only.

Setting

Range: UMODe|AMODe

Query

Range: UMOD|AMOD

*RST Setting

UMOD

Requirements

Lab Application Revision: H.01.00 and above

Programming Example

 
OUTPUT 714;"CALL:RBSetup:RLC:CONFigure UMOD"