|
Sets/queries the RLC re-establishment state. RLC re-establishment procedure typically occurs during the radio bearer setup portion of call establishment as the DPCH is reconfigured from the signalling radio bearer to the actual service configuration.
Attempting to change this setting to OFF results in the following error message: "+257, RLC behavior not compliant to 3GPP specifications for 3.4k or 13.6k SRB". When this setting is off, the test set will not perform the RLC re-establishment procedure even if the conditions would otherwise require it. This may result in unspecified behavior including loss of data.
|