Last updated: January 14, 2010
This topic is only applicable to the lab application.
|
Queries the vocoder calibration type. See Calibration Type . |
|
| Query | AOP | AIP | ICOD |
| *RST Setting | AOPath |
| Requirement | Lab Application Revision: F.00.19 and above |
OUTPUT 714;"CALL:RTVocoder:CALibration:TYPE AOP" !Set the vocoder calibration type to Audio Out Path. |
|
|
Queries the headroom of the decoded data samples to the full scale of the DAC (Digital to Analog Converter). See Real-Time Vocoder Headroom Information . |
|
| *RST Setting | 9.91E+37 (NAN) |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:DECoder:HEADroom?" !Queries decoder headroom. |
|
| Function |
Queries the headroom of the audio samples to the full scale of the ADC (Analog to Digital Converter). See Real-Time Vocoder Headroom Information . |
| *RST Setting | 9.91E+37 (NAN) |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:ENCoder:HEADroom?" !Queries encoder headroom. |
|
| Function |
Sets/queries the peak voltage of the analog audio signal that is applied at the test set's AUDIO IN connector. The units (V|mV) are optional. If no units are specified, then units default to V. See Real-Time Vocoder Headroom Information . |
| *RST Setting | 2.0 V |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:INPut:VOLTage 350mV" !Sets the peak level of Audio In signal to 350 mV. |
|
|
Sets/queries the vocoder operating mode. See Operating Mode . |
|
| Setting | Range: NORMal | CALibration |
| Query | Range: NORM | CAL |
| *RST Setting | NORMal |
| Requirement | Lab Application Revision: F.00.19 and above. |
OUTPUT 714;"CALL:RTVocoder:OPER:MODE NORM" !Sets the vocoder operating mode to Normal. |
|
| Sets the vocoder Audio Out Frequency, see Audio Out Frequency . | |
| same as setting | |
| 1000Hz | |
| Requirement | Test Application Revision: F.00.19 and above |
OUTPUT 714;"CALL:RTVocoder:OUTPut:FREQuency 1000Hz" !Sets the vocoder Audio Out Frequency to 1000Hz. |
|
| Function |
Sets/queries the maximum audio peak output level that is produced on the test set's AUDIO OUT connector according to the voice data received on the R-Traffic/R-FCH channel. The units (V|mV) are optional. If no units are specified, then units default to V. See Setting Real-Time Vocoder Parameters . |
| *RST Setting | |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:OUTPut:VOLTage 350MV" !Sets the peak level of AUDIO OUT signal to 350 mV. |
|
| Function |
Sets/queries whether or not the voice activity detection algorithm is implemented in the speech codec. See Setting Real-Time Vocoder Parameters . |
| *RST Setting | 0|OFF |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:VADetection ON" !Enable the voice activity detection algorithm. |
|
| Function |
Sets/queries the voice activity detection algorithm. See Setting Real-Time Vocoder Parameters . |
| *RST Setting | |
| Lab Application Revision: E.00.16 and above | |
OUTPUT 714;"CALL:RTVocoder:VADetection:AMRate:ALGorithm OPT2" !Select Option 2 VAD algorithm for AMR. |
|