CALL:SYSTem

CALL:SYSTem

Last updated: January 16, 2009

GPIB Command Conventions

CALL[:CELL]:SYSTem[:TYPE]?

Function

Queries the type of cell the system is emulating when in active cell mode. This command is query only because only one active cell system type (UTRA FDD) is supported at this time.

Query

Range: FDD

*RST Setting

FDD

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above.

Programming Example

 
OUTPUT 714;"CALL:CELL:SYSTEM:TYPE?"