Last updated: January 16, 2009
|
Queries an occupied bandwidth measurement result. This query returns a comma-separated list of values in the following order: integrity indicator, average occupied bandwidth, lower frequency, upper frequency. These results can also be queried individually using the FETCh:WOBWidth:INTegrity? , FETCh:WOBWidth:BANDwidth[:AVERage]? , FETCh:WOBWidth:FREQuency:LOWer? and FETCh:WOBWidth:FREQuency:UPPer? commands. If the multi-measurement state is on, the result represents the average of a number of occupied bandwidth measurements. Multi-measurement state, by default, is off. To set up multi-measurements, see SETup:WOBWidth:COUNt[:SNUMber] . |
|
OUTPUT 714;"FETCh:WOBWidth?" ! Returns integrity, occupied bandwidth, lower frequency, upper frequency. |
|
|
Queries the intermediate count of measurements completed in a multi-measurement. To set up multi-measurements, see SETup:WOBWidth:COUNt[:SNUMber] . |
|
OUTPUT 714;"FETCH:WOBWIDTH:ICOUNT?" !Returns the intermediate count of occupied bandwidth multi-measurements. |
|
|
Queries the measurement integrity indicator for the last occupied bandwidth measurement completed. Zero indicates a normal measurement. See Integrity Indicator for information about non-zero integrity results. |
|
OUTPUT 714;"FETCH:WOBWIDTH:INTegrity?" !Queries the integrity indicator for the channel occupied bandwidth results. |
|
|
Queries the average of the results of several occupied bandwidth measurements. To set the number of measurement to average, use the command SETup:WOBWidth:COUNt[:SNUMber] . |
|
OUTPUT 714;"FETCH:WOBWIDTH:BANDWIDTH:AVERAGE?" !Queries the average power for the occupied bandwidth results. |
|
|
Queries the statistical measurement results for several occupied bandwidth measurements. To set the number of measurements to gather statistics for, use the command SETup:WOBWidth:COUNt[:SNUMber] . Results are returned in the following order: minimum, maximum, average, and standard deviation occupied bandwidth. |
|
OUTPUT 714;"FETCH:WOBWIDTH:BANDWIDTH:ALL?" !Queries the statistical measurement results for occupied bandwidth measurement. |
|
|
Queries the maximum bandwidth of several occupied bandwidth measurements. To set the number of measurement to average, use the command SETup:WOBWidth:COUNt[:SNUMber] . |
|
OUTPUT 714;"FETCH:WOBWIDTH:BANDWIDTH:MAXIMUM?" !Queries the maximum occupied bandwidth result for statistical measurements. |
|
| Queries the minimum bandwidth of several occupied bandwidth measurements. To set the number of measurement to compare, use the command SETup:WOBWidth:COUNt[:SNUMber] . | |
OUTPUT 714;"FETCH:WOBWIDTH:BANDWIDTH:MINIMUM?" !Queries the minimum occupied bandwidth result for statistical measurements. |
|
|
Queries the standard deviation of several occupied bandwidth measurements. To set the number of measurement to compare, use the command SETup:WOBWidth:COUNt[:SNUMber] . |
|
OUTPUT 714;"FETCH:WOBWIDTH:BANDWIDTH:SDEVIATION?" !Queries the standard deviation of power for the occupied bandwidth measurements. |
|
|
Queries the lower frequency result of the occupied bandwidth measurement. This result can also be queried using the FETCh:WOBWidth[:ALL]? command. |
|
OUTPUT 714;"FETCh:WOBWidth:FREQuency:LOWer?" ! Queries the lower frequency result. |
|
|
Queries the upper frequency result of the occupied bandwidth measurement. This result can also be queried using the FETCh:WOBWidth[:ALL]? command. |
|
OUTPUT 714;"FETCh:WOBWidth:FREQuency:UPPer?" !Queries the upper frequency result. |
|