|
Sets/queries the multi-measurement state of the AF analyzer measurement. |
|
OUTPUT 714;"SETUP:AFANALYZER:COUNT:STATE ON" !Turns on multi-measurements. |
|
OUTPUT 714;"SETUP:AFANALYZER:DEMPHASIS:STATE ON" |
|
|
Sets/queries the detector type for audio level measurements. |
|
OUTPUT 714;"SETUP:AFANALYZER:DETECTOR:TYPE PEAK" |
|
|
Sets/queries the expandor's reference level and automatically sets the expandor's state to ON. |
|
OUTPUT 714;"SETUP:AFANALYZER:EXPANDOR:SRLEVEL 5V" !Sets expandor state to on and level to 5 V. |
|
|
Sets/queries the expandor's reference level to be used when the expandor's state is set to ON. |
|
OUTPUT 714;"SETUP:AFANALYZER:EXPANDOR:RLEVEL 5V" !Sets expandor reference level to 5 V. |
|
OUTPUT 714;"SETUP:AFANALYZER:EXPANDOR:STATE ON" |
|
|
Sets/queries the center frequency for the 100 Hz tunable bandpass filter (TBPass). |
|
10 OUTPUT 714;"SETUP:AFANALYZER:FILTER:TBPASS:FREQUENCY 300HZ" |
|
|
Sets/queries whether the audio frequency measurement is enabled. |
|
OUTPUT 714;"SETUP:AFANALYZER:FREQUENCY:STATE ON" |
|
|
Sets/queries the expected peak voltage for audio measurements. |
|
10 OUTPUT 714;SETUP:AFANALYZER:PEAK:VOLTAGE 10V" |
|
|
Sets/queries the fundamental frequency setting for the SINAD/distortion measurement. |
|
10 OUTPUT 714;SETUP:AFANALYZER:SDISTORTION:FREQUENCY 300HZ" |
|
|
Sets/queries whether the SINAD/distortion measurement is enabled. |
|
10 OUTPUT 714;SETUP:AFANALYZER:SDISTORTION:STATE ON" |
|
OUTPUT 714;"SETUP:AFANALYZER:TIMEOUT:STATE ON" |
|
|
Sets/queries the AF analyzer measurement's timeout setting to be used when the timeout state is set to ON. |
|
OUTPUT 714;"SETUP:AFANALYZER:TIMEOUT:TIME 5S" |
|