|
Sets/queries the number of audio measurements to perform at each measurement point in a single multi-measurement sweep when the SETup:SAUDio:COUNt:STATe is set to 1 (on). |
|
OUTPUT 714;"SETUP:SAUDIO:COUNT:NUMBER 5" !Makes 5 measurements at each frequency point in the sweep. |
|
|
Selects/queries the swept audio measurement's multi-measurement count state. |
|
OUTPUT 714;"SETUP:SAUDIO:COUNT:STATE ON" !Turns on multi-measurement for the swept audio measurement. |
|
|
Sets/queries the audio generator's coupling to the AUDIO OUT port. |
|
| DC | |
OUTPUT 714;"SETUP:SAUDIO:COUPLING AC" !Select AC coupling to the AUDIO OUT port. |
|
|
Sets/queries the type of level detector used in swept audio measurements. |
|
| RMS | |
OUTPUT 714;"SETUP:SAUDIO:DETECTOR:TYPE PEAK" !Select the peak detector for the AF analzyer. |
|
|
Returns a comma-separated list of the generated frequency for each frequency point (see SETup:SAUDio:FREQuency:POINts ). When you specify the start frequency, stop frequency, and the number of measurement points, the test set calculates the intermediate frequencies that are generated. You cannot directly set the intermediate frequencies using this command, you can only query them. |
|
OUTPUT 714;"SETUP:SAUDIO:FREQUENCY:VALUE?" !Queries the list of generated frequencies. |
|
|
Sets/queries the expected peak voltage of the swept audio measurement. This determines the range and resolution of the sampled voltage values. |
|
OUTPUT 714;"SETUP:SAUDIO:PEAK:VOLTAGE 5V" |
|
| Selects/queries the swept audio measurement timeout state. Timeout is set using the SETup:SAUDio:TIMeout:TIME command. | |
OUTPUT 714;"SETUP:SAUDIO:TIMEOUT:STATE ON" !Enables timeouts for swept audio measurements. |
|