Last updated: January 16, 2009
|
Sets/queries the power control algorithm for uplink channels. This setting is useful only when the test segment is set to Manual (see SETup:WILPower:SEGment ) and the start power is different from the stop power. See Inner Loop Power Measurement Description for more information. |
|
OUTPUT 714;"SETup:WILPower:ALGorithm ALG1" !Sets Power control algorithm to use algorithm 1. |
|
|
Sets/queries Maximum Output Power Test Tolerance .
This setting is only applicable when |
|
| Same as setting | |
| 0.7 dB | |
OUTPUT 714;"SETup:WILPower:MAXimum:OUTPut:POWer:TEST:TOLerance 0.8" ! Sets Maximum Output Power Test Tolerance to 0.8 dB. |
|
|
Sets/queries the Maximum Power Threshold for Test Control .
This setting is only applicable when
When |
|
| 1 (auto) | |
OUTPUT 714;"SETup:WILPower:MAXimum:POWer:THReshold:TEST:CONTrol:AUTO OFF" ! Sets Maximum Power Threshold for Test Control to Manual. |
|
|
Sets/queries Maximum Power Threshold for Test Manual .
This setting is only applicable when |
|
| Same as setting | |
| +21.00 dBm | |
OUTPUT 714;"SETup:WILPower:MAXimum:POWer:THReshold:TEST:MANual +19" ! Sets Maximum Power Threshold for Test Manual to +19 dBm. |
|
|
Sets/queries Minimum Output Power Test Tolerance .
This setting is only applicable when |
|
| Same as setting | |
| 1.0 dB | |
OUTPUT 714;"SETup:WILPower:Minimum:OUTPut:POWer:TEST:TOLerance 0.8" ! Sets Minimum Output Power Test Tolerance to 0.8 dB. |
|
|
Sets/queries the Minimum Power Threshold for Test Control .
This setting is only applicable when
When |
|
| 0 (manual) | |
OUTPUT 714;"SETup:WILPower:Minimum:POWer:THReshold:TEST:CONTrol:AUTO ON" ! Sets Minimum Power Threshold for Test Control to Auto. |
|
|
Sets/queries Minimum Power Threshold for Test Manual .
This setting is only applicable when |
|
| Same as setting | |
| -49.00 dBm | |
OUTPUT 714;"SETup:WILPower:Minimum:POWer:THReshold:TEST:MANual -50" ! Sets Minimum Power Threshold for Test Manual to -50 dBm. |
|
|
Sets/queries UE Range Time Control . |
|
| Range: 1|0 | |
| 1 (auto) | |
OUTPUT 714;"SETup:WILPower:MS:RANGe:TIME:CONTrol:AUTO 1" ! Sets UE Range Time Control to Auto. |
|
|
Sets/queries Manual UE Range Time . This setting is only applicable when SETup:WILPower:MS:RANGe:TIME:CONTrol:AUTO is set to manual (0|OFF). |
|
| Same as setting | |
| 0 s | |
OUTPUT 714;"SETup:WILPower:MS:RANGe:TIME:MANual 0" ! Sets Manual UE Range Time to 0 seconds. |
|
|
Sets/queries the number of timeslots to be measured which equals to the total number of TPC commands sent for the chosen test segments. This setting is used only during two test configurations: when Test Segment A is selected and when Test Segment Manual is selected with Start Power and Stop Power set to the same values. See Inner Loop Power Measurement Description for more information. The following sequence of TPC commands are sent in accordance with the selected number of timeslots: |
|
| S45 | |
OUTPUT 714;"SETup:WILPower:NSLOts S60" !Sets the number of timeslots to be measured to 60. |
|
|
Sets/queries the Inner Loop Power control measurement configuration. With Manual selected, you can build a custom test segment to run. If you select a test segment other than Manual, the test set will run a single test segment as specified in the standard (referred to as Test Steps in the standard). See Inner Loop Power Measurement Description for more information. |
|
| A | |
OUTPUT 714;"SETup:WILPower:SEGment MAN" !Sets the segment to be measured to manual. |
|
|
Sets/queries the power control step size for the UE transmitter which is the change in the UE transmitter output power in response to a single TPC_cmd derived at UE. ONE is the change of 1 dB and TWO is the change of 2 dB. This setting is useful only when the test segment is set to Manual (see SETup:WILPower:SEGment ) and the power control algorithm is set to ALG1 (see SETup:WILPower:ALGorithm . See Inner Loop Power Measurement Description for more information. |
|
OUTPUT 714;"SETup:WILPower:STEP ONE" !Sets Power control step size to 1 dB. |
|
|
Sets/queries the start power for the measurement in manual mode (see SETup:WILPower:SEGment ). The UE will be instructed to the start power and make the measurements while ramping up/down the power to the specified stop power. See Inner Loop Power Measurement Description for more information. |
|
|
Range: -61 dBm to +30 dBm (-50 dBm to +24 dBm for Class 1 UE) |
|
|
Range: -61 dBm to +30 dBm (-50 dBm to +24 dBm for Class 1 UE) |
|
OUTPUT 714;"SETup:WILPower:STARt 10" !Sets Power control algorithm to use algorithm 1. |
|
|
Sets/queries the stop power for the measurement in manual mode (see SETup:WILPower:SEGment ). The UE will be instructed to the start power and make the measurements while ramping up/down the power to the specified stop power. See Inner Loop Power Measurement Description for more information. |
|
|
Range: -61 dBm to +30 dBm (-50 dBm to +24 dBm for Class 1 UE) |
|
|
Range: -61 dBm to +30 dBm (-50 dBm to +24 dBm for Class 1 UE) |
|
OUTPUT 714;"SETup:WILPower:STOP 0" |
|
|
The setting form of this command performs two functions: (1) sets the Inner Loop Power control measurement's timeout (see Measurement Timeouts ) value, and (2) sets the Inner Loop Power control measurement's timeout STATe to 1 (on). The query form returns the Inner Loop Power control measurement's timeout value. |
|
OUTPUT 714;"SETUP:WILPOWER:TIMEOUT:STIME 5 S" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the Inner Loop Power control measurement's timeout (see Measurement Timeouts ) state. |
|
OUTPUT 714;"SETUP:WILPOWER:TIMEOUT:STATE ON" |
|
|
Sets/queries the Inner Loop Power control measurement's timeout (see Measurement Timeouts ) setting to be used when the timeout state is set to ON. |
|
OUTPUT 714;"SETUP:WILPOWER:TIMEOUT:TIME 5 S" |
|
| Function |
Setting/Query Range (Resolution = 0.01 dB) |
*RST Setting | |
| See Transmitter Power Control Pass/Fail Ranges . | |||
| SETup:WILPower:TPCRange[:SINGle]:STEP:DOWN:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Sngl Step Down 1dB: Lwr Lim | 0.00 to -1.00 dB | -0.40 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:DOWN:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Sngl Step Down 1dB: Upr Lim | -1.00 to -2.00 dB | -1.60 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:DOWN:DB2:LIMit:LOWer | TX Pwr Ctrl Rng Sngl Step Down 2dB: Lwr Lim | 0.00 to -2.00 dB | -0.85 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:DOWN:DB2:LIMit:UPPer | TX Pwr Ctrl Rng Sngl Step Down 2dB: Upr Lim | -2.00 to -4.00 dB | -3.15 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:NONE:LIMit:LOWer | TX Pwr Ctrl Rng Sngl Step None: Lwr Lim | 0.00 to -1.00 dB | -0.60 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:NONE:LIMit:UPPer | TX Pwr Ctrl Rng Sngl Step None: Upr Lim | 0.00 to +1.00 dB | +0.60 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:UP:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Sngl Step Up 1dB: Lwr Lim | 0.00 to +1.00 dB | +0.40 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:UP:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Sngl Step Up 1dB: Upr Lim | +1.00 to +2.00 dB | +1.60 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:UP:DB2:LIMit:LOWer | TX Pwr Ctrl Rng Sngl Step Up 2dB: Lwr Lim | 0.00 to +2.00 dB | +0.85 dB |
| SETup:WILPower:TPCRange[:SINGle]:STEP:UP:DB2:LIMit:UPPer | TX Pwr Ctrl Rng Sngl Step Up 2dB: Upr Lim | +2.00 to +4.00 dB | +3.15 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:DOWN:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg1 Step Down 1dB: Lwr Lim | -6.00 to -10.00 dB | -7.70 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:DOWN:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg1 Step Down 1dB: Upr Lim | -10.00 to -14.00 dB | -12.30 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:DOWN:DB2:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg1 Step Down 2dB: Lwr Lim | -12.00 to -20.00 dB | -15.70 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:DOWN:DB2:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg1 Step Down 2dB: Upr Lim | -20.00 to -28.00 dB | -24.30 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:UP:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg1 Step Up 1dB: Lwr Lim | +6.00 to +10.00 dB | +7.70 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:UP:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg1 Step Up 1dB: Upr Lim | +10.00 to +14.00 dB | +12.30 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:UP:DB2:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg1 Step Up 2dB: Lwr Lim | +12.00 to +20.00 dB | +15.70 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm1:STEP:UP:DB2:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg1 Step Up 2dB: Upr Lim | +20.00 to +28.00 dB | +24.30 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:DOWN:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg2 Step Down 1dB: Lwr Lim | -5.70 dB | |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:DOWN:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg2 Step Down 1dB: Upr Lim | -10.00 to -18.00 dB | -14.30 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:NONE:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg2 Step None: Lwr Lim | 0.00 to -2.00 dB | -1.10 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:NONE:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg2 Step None: Upr Lim | 0.00 to +2.00 dB | +1.10 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:UP:DB1:LIMit:LOWer | TX Pwr Ctrl Rng Agg Alg2 Step Up 1dB: Lwr Lim | +2.00 to +10.00 dB | +5.70 dB |
| SETup:WILPower:TPCRange:AGGRegate:ALGorithm2:STEP:UP:DB1:LIMit:UPPer | TX Pwr Ctrl Rng Agg Alg2 Step Up 1dB: Upr Lim | +10.00 to +18.00 dB | +14.30 dB |
OUTPUT 714;"SETup:WILPower:TPCRange:STEP:DOWN:DB1:LIMit:LOWer -0.45" ! Sets TX Pwr Ctrl Rng Sngl Step Down 1dB: Lwr Lim to -0.45 dB. |
|||
|
Sets/queries the Inner Loop Power control measurement's Trigger Delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed. |
|
OUTPUT 714;"SETUP:WILPOWER:TRIGGER:DELAY 1MS" |
|