Last updated: January 16, 2009
|
Sets/queries the Off Power Limit (see Off Power Limit ). |
|
| Requirements | |
OUTPUT 714;"SETup:WOOPower:OFF:POWer:LIMit -54" ! Sets the Off Power Limit to -54 dBm. |
|
|
This command sets symmetrical upper and lower pass/fail limits for the difference between the "on" power and the expected power.
|
|||
| Requirements | |||
| 9.0 dB | |||
OUTPUT 714;"SETup:WOOPower:OPEN:LOOP:POWer:LIMit 10" ! Sets the Open Loop Power Error Upper and Lower Limits to 10 dB. |
|||
|
Sets/queries the Open Loop Power Error Upper Limit (see Open Loop Power Error Upper Limit ). |
|
| Requirements | |
| 9.0 dB | |
OUTPUT 714;"SETup:WOOPower:OPEN:LOOP:POWer:UPPer:LIMit 10" ! Sets the Open Loop Power Error Upper Limit to 10 dB. |
|
|
Sets/queries the Open Loop Power Error Lower Limit (see Open Loop Power Error Lower Limit ). |
|
| Requirements | |
| -9.0 dB | |
OUTPUT 714;"SETup:WOOPower:OPEN:LOOP:POWer:LOWer:LIMit -10" ! Sets the Open Loop Power Error Lower Limit to -10 dB. |
|
|
The setting form of this command performs two functions: (1) sets the PRACH transmit on/off power measurement's timeout value (see Measurement Timeouts ), and (2) sets the timeout STATe to 1 (on). The query form returns the PRACH transmit on/off power measurement's timeout value. |
|
| Requirements | |
| Same as setting | |
OUTPUT 714;"SETup:WOOPower:TIMeout 5" !Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the PRACH transmit on/off power measurement's timeout state (see Measurement Timeouts ). |
|
| Requirements | |
OUTPUT 714;"SETup:WOOPower:TIMeout:STATe ON" |
|
|
Sets/queries the PRACH transmit on/off power measurement's timeout setting (see Measurement Timeouts ) to be used when the timeout state is set to ON. |
|
| Requirements | |
OUTPUT 714;"SETup:WOOPower:TIMeout:TIME 5" |
|