Last updated: January 16, 2009
|
Sets/queries the spectrum emission mask multi-measurement state. |
|
OUTPUT 714;"SETUP:WSEMASK:COUNT:STATE ON" ! Turns on spectrum emission mask multi-measurements. |
|
|
The setting form of this command performs two functions: (1) sets the spectrum emission mask measurement's timeout (see Measurement Timeouts ) value, and (2) sets the spectrum emission mask measurement's timeout STATe to 1 (on). The query form returns the spectrum emission mask measurement's timeout value. |
|
OUTPUT 714;"SETUP:WSEMASK:TIMEOUT:STIME 5 S" ! Sets timeout state to ON and sets the timeout time to 5 seconds. |
|
|
Sets/queries the spectrum emission mask measurement's timeout (see Measurement Timeouts ) state. |
|
OUTPUT 714;"SETUP:WSEMASK:TIMEOUT:STATE ON" |
|
|
Sets/queries the spectrum emission mask measurement's timeout (see Measurement Timeouts ) setting to be used when the timeout state is set to ON. |
|
OUTPUT 714;"SETUP:WSEMASK:TIMEOUT:TIME 5 S" |
|
|
Sets/queries the SEM measurement's
HS-DPCCH Trigger Subframe Alignment
This command is only applicable when
SETup:WSEMask:TRIGger:SOURce
is set to |
|
| Same as setting | |
| 0 (subframe 0) | |
|
Test Application Revision: A.08 and above with the required feature license |
|
OUTPUT 714;"SETup:WSEMask:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 1" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 1. |
|
|
Sets/queries the spectrum emission mask measurement's Trigger Delay setting. This setting can be used to delay the measurement trigger in order to start a measurement during a specific timeslot in the frame. For example, a 1.333 ms delay would cause the trigger to wait until after the first two timeslots have elapsed. |
|
| Same as setting | |
|
Test Application Revision: A.02 and above Test Application Revision A.08 and Lab Application C.03, increased range to -12 to 12 ms (previously it was -10 ms to 10 ms) |
|
OUTPUT 714;"SETUP:WSEMASK:TRIGGER:DELAY 1MS" |
|
|
Sets/queries the spectrum emission mask measurement's Trigger Source . |
|
| AUTO | |
|
Test Application Revision: A.02 and above Test Application Revision A.08 with the required feature license and Lab Application C.03, added HSDPcchannel |
|
OUTPUT 714;"SETUP:WSEMASK:TRIGGER:SOURCE IMMEDIATE" |
|