Last updated: January 16, 2009
|
Sets/queries Power Step Size . |
|
| Same as setting | |
| -4.00 dB | |
OUTPUT 714;"SETup:WTDPower:STEP -5" ! Sets the power step size to -5 dB. |
|
|
Sets/queries Number of Power Steps .
The total number of power results returned by the measurement is 1 + |
|
| Same as setting | |
| 19 | |
OUTPUT 714;"SETup:WTDPower:STEP:COUNt 5" ! Sets the number of power steps to 5. |
|
|
Sets/queries the Power Step Time . |
|
| Same as setting | |
| MS20 | |
OUTPUT 714;"SETup:WTDPower:STEP:TIME MS40" ! Sets power step time to 40 ms. |
|
|
The setting form of this command performs two functions: (1) sets the measurement timeout value (see SETup:WTDPower:TIMeout:TIME ), and (2) sets the measurement timeout state to on (see SETup:WTDPower:TIMeout:STATe ). The query form of this command returns the measurement timeout value. See Measurement Timeouts . |
|
| Same as setting | |
OUTPUT 714;"SETup:WTDPower:TIMeout 5" ! Sets timeout state to on and sets the timeout time to 5 seconds. |
|
|
Sets/queries the measurement timeout state. The measurement timeout state can also be set to on using the SETup:WTDPower:TIMeout[:STIMe] command. See Measurement Timeouts . |
|
OUTPUT 714;"SETup:WTDPower:TIMeout:STATe ON" |
|
|
Sets/queries the measurement timeout value to be used when the timeout state is set to on. The measurement timeout value can also be set using the SETup:WTDPower:TIMeout[:STIMe] command. See Measurement Timeouts . |
|
| Same as setting | |
OUTPUT 714;"SETup:WTDPower:TIMeout:TIME 5" |
|