Last updated: November 17, 2010
|
Sets/queries the multi-measurement state of the waveform quality measurement. |
|
OUTPUT 714;"SETUP:WWQUALITY:COUNT:STATE ON" ! Turns on multi-measurements. |
|
|
Sets/queries HS-DPCCH Measurement Interval . This command is only applicable when SETup:WWQuality:TRIGger:SOURce = HSDPcchannel.
The sum of |
|
| Same as setting | |
| 1.0 slot | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WWQuality:INTerval:HSDPcchannel 0.8" ! Sets HS-DPCCH Measurement Interval to 0.8 slot. |
|
|
Sets/queries the waveform quality measurement's timeout state. |
|
OUTPUT 714;"SETUP:WWQUALITY:TIMEOUT:STATE ON" |
|
|
Sets/queries the waveform quality measurement's timeout setting to be used when the timeout state is set to ON. |
|
OUTPUT 714;"SETUP:WWQUALITY:TIMEOUT:TIME 5S" |
|
|
Sets/queries Transient Period . |
|
| INCL (include) | |
|
Test Application Revision: A.09 and above, with the required feature license Lab Application Revision: C.04 and above Lab Application Revision: D.00 and above Test Application Revision A.10 and Lab Application D.01, this command is now applicable for all Trigger Source settings (non-HSDPA as well as HSDPA) |
|
OUTPUT 714;"SETup:WWQuality:TRANsient EXCLude" ! Sets Transient Period to Exclude. |
|
|
Sets/queries HS-DPCCH Trigger Slot Alignment . This command is only applicable when SETup:WWQuality:TRIGger:SOURce = HSDPcchannel. |
|
| ACKN | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WWQuality:TRIGger:ALIGnment:HSDPcchannel:SLOT CQI1" ! Sets HS-DPCCH Trigger Slot Alignment to CQI1. |
|
|
Sets/queries HS-DPCCH Trigger Subframe Alignment . This command is only applicable when SETup:WWQuality:TRIGger:SOURce = HSDPcchannel. |
|
| Same as setting. | |
| 0 | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WWQuality:TRIGger:ALIGnment:HSDPcchannel:SUBFrame 3" ! Sets HS-DPCCH Trigger Subframe Alignment to subframe 3. |
|
|
Sets/queries HS-DPCCH Trigger Subslot Alignment . This command is only applicable when SETup:WWQuality:TRIGger:SOURce = HSDPcchannel.
The sum of |
|
| Same as setting. | |
| 0.0 slot | |
|
Test Application Revision: A.09 and above, with the required feature license |
|
OUTPUT 714;"SETup:WWQuality:TRIGger:ALIGnment:HSDPcchannel:SUBSlot 0.3" ! Sets HS-DPCCH Trigger Subslot Alignment to 0.3 slot. |
|
|
Sets/queries Trigger Source . |
|
| AUTO | |
|
Test Application Revision: A.02 and above. Test Application Revision A.09, with the required feature license, added HSDPcchannel. Lab Application Revision: A.01 and above. Lab Application Revision C.04, D.00, added HSDPcchannel. Lab Application Revision F.00, added EFRame. Test Application Revision A.14, with the required feature license, added EFRame. |
|
OUTPUT 714;"SETUP:WWQUALITY:TRIGGER:SOURCE AUTO" |
|
|
Sets/queries Timeslot . This command is only applicable when SETup:WWQuality:TRIGger:SOURce is NOT set to HSDPcchannel. |
|
| Same as setting | |
OUTPUT 714;"SETUP:WWQUALITY:TSLOT 10" |
|