|
Queries the name of the currently running application. To query the revision of the currently running application, see SYSTem:APPLication[:CURRent]:REVision? . To switch applications, see SYSTem:APPLication:SELect[:NAME] and SYSTem:APPLication:SELect:REVision . |
|
|
Range: See SYSTem:APPLication:CATalog[:NAME]? . |
|
OUTPUT 714;"SYSTem:APPLication?" |
|
|
Queries the revision of the currently running application. To query the name of the currently running application, see SYSTem:APPLication[:CURRent][:NAME]? . To switch to a different revision of an application, see SYSTem:APPLication:SELect[:NAME] and SYSTem:APPLication:SELect:REVision . |
|
|
Range: 0 to 20 characters from the set .0123456789aAbBcCdDeEfF, enclosed by double quotes. For example, "A.01.01" |
|
OUTPUT 714;"SYSTem:APPLication:REVision?" |
|
|
Queries the names of the applications stored on the test set (whether they are licensed or not). This query returns a comma-separated list of double-quoted strings (one for each application stored on the test set). To query the number of applications stored on the test set, see SYSTem:APPLication:CATalog[:NAME]:COUNt? . To switch applications, see SYSTem:APPLication:SELect[:NAME] and SYSTem:APPLication:SELect:REVision . |
|
|
Range: One or more of the following strings, separated by commas - |
|
| Query (continued) |
|
OUTPUT 714;"SYSTem:APPLication:CATalog?" |
|
|
Queries the total number of applications stored on the test set. To query the names of the applications stored on the test set, see SYSTem:APPLication:CATalog[:NAME]? . |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:COUNt?" |
|
|
Queries the names of the formats in the current application. This query returns a comma-separated list of double-quoted strings (one for each format in the application). To query the number of formats in the current application, see SYSTem:APPLication:CATalog:FORMat:COUNt? . To switch formats in a fast switching application, see SYSTem:APPLication:FORMat[:NAME] . |
|
|
Range: One or more of the following strings separated by commas - |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:FORMat?" |
|
|
Queries the number of formats in the current application. To query the names of the formats in the current application, see SYSTem:APPLication:CATalog:FORMat? . |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:FORMat:COUNt?" |
|
|
Queries the license status for the specified application/revision. The application/revision does not have to be installed in the test set. The query must include a parameter for the application name and revision, enclosed by single quotes and separated by a comma. For application names and revisions, see SYSTem:APPLication:CATalog[:NAME]? and SYSTem:APPLication:CATalog:REVision?<sp>'<application name>' . Note that the application name and revision parameters are not case-sensitive. |
|
|
|
OUTPUT 714;"SYSTem:APPLication:CATalog:LICense? 'CDMA 2000 Mobile Test','B.07.00'" |
|
|
Queries the names of the applications, formats and features that are licensed for the test set. The applications, formats and features do not have to be installed in the test set to be returned by this query. This query returns a comma-separated list of double-quoted strings (two for each application, one for each format or feature). To query the number of licensed applications, formats and features for the test set, see SYSTem:APPLication:CATalog:LICense:APPLication:COUNt? . |
|
|
Range: One or more of the following strings, separated by commas -
|
|
| Query (continued) |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:LICense:APPLication:ALL?" |
|
|
Queries the number of applications, formats and features that are licensed for the test set. The applications, formats and features do not have to be installed in the test set to be included in the query result. To query the names of the licensed applications, formats and features for the test set, see SYSTem:APPLication:CATalog:LICense:APPLication:ALL? . |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:LICense:APPLication:COUNt?" |
|
|
Queries the coverage date of the installed R2C license. See Test Application Revision To Current (R2C) license . |
|
| Range: three comma-separated values with the format <year>, <month>, <day>. | |
| Test Application Revision: A.14.16 and above | |
OUTPUT 714;"SYSTem:APPLication:CATalog:R2Current:COVerage?" ! Queries the coverage date of the installed R2C license. |
|
|
Queries the R2C license status. See Test Application Revision To Current (R2C) license . |
|
| LIC | NLIC | PART | |
| Test Application Revision: A.14.16 and above | |
OUTPUT 714;"SYSTem:APPLication:CATalog:R2Current:STATus?" ! Queries the R2C license status. |
|
|
Queries the revisions stored on the test set for the specified application. The query must include a parameter for the application name enclosed by single quotes. For application names, see SYSTem:APPLication:CATalog[:NAME]? . Note that the application name parameter is not case-sensitive. This query returns a comma-separated list of double-quoted strings (one for each revision of the application). Note, if you have several revisions of the application stored on the test set, you may need to increase your GPIB controller's timeout time to avoid a timeout condition. To query the number of revisions stored on the test set for the specified application, see SYSTem:APPLication:CATalog:REVision:COUNt?<sp>'<application name>' . To switch to a different revision of an application, see SYSTem:APPLication:SELect[:NAME] and SYSTem:APPLication:SELect:REVision . |
|
| Range: Comma-separated list of 0 to 20 characters from the set .0123456789aAbBcCdDeEfF, enclosed by double quotes. For example, "A.01.01","A.02.01" | |
OUTPUT 714;"SYSTem:APPLication:CATalog:REVision? 'CDMA 2000 MOBILE TEST'" |
|
|
Queries the number of revisions stored on the test set for the specified application. The query must include a parameter for the application name enclosed by single quotes. For application names, see SYSTem:APPLication:CATalog[:NAME]? . Note that the application name parameter is not case-sensitive. To query the revision numbers stored on the test set for the specified application, see SYSTem:APPLication:CATalog:REVision?<sp>'<application name>' . |
|
OUTPUT 714;"SYSTem:APPLication:CATalog:REVision:COUNt? 'CDMA 2000 MOBILE TEST'" |
|
|
Switches to the specified format (in the current application). Only fast switching applications include more than one format. To determine what formats are available in the current application, see SYSTem:APPLication:CATalog:FORMat? . To determine the license status of a format, see SYSTem:APPLication:FORMat:LICense?<sp>'<format name>' . Queries the name of the currently active format in the current application. |
|
|
Note: The query result is returned within a pair of double quotation marks. For example, if the current application is GSM/GPRS, the test set returns |
|
OUTPUT 714;"SYSTem:APPLication:FORMat 'IS-2000/IS-95/AMPS'" OUTPUT 714;"SYSTem:APPLication:FORMat?" |
|
|
Queries the license status of the specified format in the current application. The query must include a parameter for the format name enclosed by single quotes. For format names, see SYSTem:APPLication:CATalog:FORMat? . Note that the format name parameter is not case-sensitive. |
|
OUTPUT 714;"SYSTem:APPLication:FORMat:LICense? 'IS-2000/IS-95/AMPS'" |
|
|
Switches to the specified application (this includes a reboot of the test set). To determine what applications are stored on the test set, see SYSTem:APPLication:CATalog[:NAME]? . The revision that is switched to is determined by SYSTem:APPLication:SELect:REVision . To determine the license status of the application/revision, see SYSTem:APPLication:CATalog:LICense?<sp>'<application name>','<revision>' . Queries the name of the application that will be loaded after the next reboot of the test set. |
|
|
Range: See SYSTem:APPLication:CATalog[:NAME]? . |
|
|
Range: See SYSTem:APPLication:CATalog[:NAME]? . |
|
OUTPUT 714;"SYSTem:APPLication:SELect 'CDMA 2000 MOBILE TEST'" OUTPUT 714;"SYSTem:APPLication:SELect?" |
|
|
Sets the revision that will be loaded when the application is switched to using the SYSTem:APPLication:SELect[:NAME] command. To determine what application is to be switched to, see SYSTem:APPLication:SELect[:NAME] . To determine what revisions are stored on the test set for the specified application, see SYSTem:APPLication:CATalog:REVision?<sp>'<application name>' . To determine the license status of a revision, see SYSTem:APPLication:CATalog:LICense?<sp>'<application name>','<revision>' . To query the revision that will be loaded when an application is switched to, see SYSTem:APPLication:SELect:REVision?<sp>'<application name>' .
|
|||
|
Range: see SYSTem:APPLication:CATalog[:NAME]? and SYSTem:APPLication:CATalog:REVision?<sp>'<application name>' . |
|||
OUTPUT 714;"SYSTem:APPLication:SELect:REVision 'CDMA 2000 Mobile Test','B.06.30'" |
|||
|
Queries the revision that will be loaded when the specified application is switched to using the SYSTem:APPLication:SELect[:NAME] command. The query must include a parameter for the application name enclosed by single quotes. For application names, see SYSTem:APPLication:CATalog[:NAME]? . Note that the application name parameter is not case-sensitive. To set the revision that will be loaded when the specified application is switched to, see SYSTem:APPLication:SELect:REVision .
|
|||
| Range: 0 to 20 characters from the set .0123456789aAbBcCdDeEfF, enclosed by double quotes. For example, "A.01.01" | |||
OUTPUT 714;"SYSTem:APPLication:SELect:REVision? `CDMA 2000 MOBILE TEST'" |
|||