Home > SYSTem:DATE
Last updated: January 16, 2009
GPIB Command Conventions
Function
Sets/queries the date.
Setting
Range:
Query
*RST Setting
Requirements
Test or Lab Application Revision: A.01 and above
Programming Example
OUTPUT 714;"SYSTEM:DATE 2001,9,27" !Sets the date to September 27,2001.
OUTPUT 714;"SYSTEM:DATE? !Returns "+2001,+9,+27" if the date has been set to September 27,2001.
SYSTem:UTC:DATE