SYSTem:ROSCillator

SYSTem:ROSCillator

Last updated: January 16, 2009

GPIB Command Conventions

SYSTem:ROSCillator[:TIMebase]?

Function

Queries the timebase source.

If an external timebase is used, it must have these characteristics:

  • an output level of 0 to +13 dBm

  • frequency of 10 MHz

Query

Range:

INT = internal source

EXT = external source

Requirements

Test or Lab Application Revision: A.01 and above

SYSTem:ROSCillator:LOCKed?

Function

Queries the timebase to find out if it is locked or unlocked. Returns 0 or 1.

Query

Range:

0 = unlocked

1 = locked

Requirements

Test or Lab Application Revision: A.01 and above