Last updated: January 16, 2009
This section is only applicable to the lab application.
|
This query returns an integer value of 1 if the status of the test set's protocol logging data source is:
See CALL:PLOGging<:STATus|:STATe>? . If the state of the test set's protocol logging data source is not Active, this query will "hang" until a transition to the Active state occurs, or a bus timeout or device clear terminates the query attempt. |
|
| Requirements | Lab Application Revision: A.01.20 and above |
| Range: 1 | |
| OUTPUT 714;"CALL:PLOGGING:ACT?"!Queries the Active state. |
|
This query returns an integer value of 1 if the status of the test set's protocol logging data source is either:
See CALL:PLOGging<:STATus|:STATe>? . If the state of the test set's protocol logging data source is not one of the above, this query will "hang" until a transition to one of these states occurs, or a bus timeout or device clear terminates the query attempt. |
|
| Requirements | Lab Application Revision: A.01.20 and above |
| Range: 1 | |
| OUTPUT 714;"CALL:PLOGGING:CONN?"!Queries the connected state. |
|
This query returns an integer value of 1 if the status of the test set's protocol logging data source is either:
See CALL:PLOGging<:STATus|:STATe>? . If the state of the test set's protocol logging data source is not one of the above, this query will "hang" until a transition to one of these states occurs, or a bus timeout or device clear terminates the query attempt. |
|
| Requirements | Lab Application Revision: A.01.20 and above |
| Range: 1 | |
| OUTPUT 714;"CALL:PLOGGING:DONE?"!Queries the done (logging) state. |
|
This command will cause the test set to transition to the Active logging state. Once in the Active Logging state the test set can begin forwarding messages to the protocol logging software. The protocol logging software must be in real-time mode (not post-capture mode) and a real-time logging session must be connected before transition to the Active logging state is possible. A real-time logging session is connected by entering the IP Address of the test set in the Tools, Configuration window found in the protocol logging software. When a real-time logging session is connected, the test set's front panel logging annunciator will display Logging:Idle (see the Idle description in CALL:PLOGging<:STATus|:STATe>? .) After the transition from the Idle to Active logging state has occurred, the test set's front paned logging annunciator will appear as follows: The test set can also be transitioned to the Active logging state by clicking on the REC (record) button located in the protocol logging software |
|||||
| Requirements | Lab Application Revision: A.01.20 and above | ||||
| OUTPUT 714;"CALL:PLOGGING:START" !Starts protocol logging. |