Activating Protocol Logging From the Test Set
Last updated: January 16, 2009
This section is only applicable to the lab application.
Once a connection is established between the PC running the WPA (Wireless Protocol Advisor) and the test set, a logging session can be activated (or deactivated) by selecting the start (or stop) softkey from the test set's front panel or by sending GPIB commands that perform the same functions:
The WPA software performs the same start/stop functions when the REC (RECord) button is selected. Refer to the WPA on-line Help for details.
Test Set Control of Protocol Logging
If a PC with the WPA software has not yet connected with the test set, an error message will be generated if an attempt is made to start protocol logging. Exactly one PC/WPA can be connected to a test set at one time.
Front Panel Control of Protocol Logging
-
Press the
CALL SETUP
key to go to the
Call Setup
screen.
-
Press the
More
key on the left hand
Call Control
menu to go to menu 3.
-
Select
Protocol Logging
(
F1
).
-
Select
Start Protocol Logging
(
F1
) to begin logging.
Remote Control of Protocol Logging
The GPIB command to control Protocol Logging is
CALL:PLOGging
.