Revision History

This page tracks changes made in each release of Keysight MCP Server for Instrument Control.

Version Date Change
Assure 1.1 October 2026

Platform & Installation

  • Added Linux as a supported platform, with its own installer and the same auto-generated AI client configuration files as Windows. On Linux, instruments are reached through a direct LAN connection; GPIB, USB, and serial (RS-232) instruments, and connection through Keysight IO Libraries Suite, NI-VISA, or R&S VISA, aren't supported there yet. See Getting Started.
  • Installer now auto-generates MCP client configuration files for Claude Code, Claude Desktop, VS Code (GitHub Copilot), and Cursor, placed in a client-configs folder with a README.txt.

Instrument & Workflow Support

  • Instruments with no IDF (non-Keysight Technologies, or unpublished virtual instruments) now degrade gracefully instead of hard-failing; discover_instruments flags non-Keysight Technologies instruments up front. See Workflow.

Tools

  • Every tool now carries MCP tool annotations (Read-only, Destructive, Idempotent, Open World), letting an AI client decide automatically how to handle a given tool call. See Tools.
  • New describe_commands tool for translating a SCPI sequence from one instrument model to another, by recovering each command's real meaning from the source model's IDF before resolving the equivalent on the target model. See Tools.
  • Removed list_procedures and resolve_procedure. Procedure search and listing now happen through search_instrument_capabilities. Tool count: 19 to 17.
  • preview_commands now validates SCPI the engineer supplies directly, in either short or long form, instead of only sequences Assure generated itself. For an instrument with no matching IDF, it checks any commands it recognizes as universal (such as *IDN? and *OPC?) and marks the rest as unchecked, rather than blocking the preview. See Tools.
  • Resolving and previewing a SCPI sequence no longer requires the instrument to be connected or powered on. Only execute_commands needs the instrument reachable; if it isn't, the tool reports a clear timeout with suggested checks (power, LAN status, cabling, network path) instead of failing silently. See Tools.

Defects Fixed

  • Fixed an issue where searching for procedures incorrectly required specifying an instrument model.
  • Fixed an issue where some SCPI parameter enum values defined in an instrument's IDF (for example, sweep modes or step lists) were missing from search results and command resolution.
  • Fixed an issue where long instructions sent to the MCP server could be truncated.
  • Fixed IDF matching so firmware version strings using wildcard placeholders resolve correctly.
  • Fixed an issue where instrument discovery intermittently returned only instruments known to Keysight Connection Expert, omitting other auto-discovered devices.
  • Fixed binary data handling over the direct socket connection method, affecting waveform file transfers and some query responses.
  • Fixed a momentary flashing background window during Windows installation.

Security

  • Updated underlying Go package dependencies to address known security vulnerabilities identified by routine scanning.
0.1 May 2026 Initial release: NLP-to-SCPI pipeline, 18 MCP tools, 6 built-in procedures, operation tracking, file transfer, and update management.