Messages

Messages provide information about the status of the instrument or an action that has been performed (for example, Calibration is complete). Messages also appear to inform you of errors that may have occurred. Instrument messages are:

  • Displayed in the Message Area, which is located at the bottom of the display.
  • Listed in the Message Log Viewer dialog. Click Help > View Message Log.
  • Many of the messages can also be remotely queried using the :SYSTem:ERRor:NEXT? command.
Displayed Message Type Icons
Icon Description
Operational error messages indicate instrument hardware or software failures. This type of message will remain on the display until the error condition is corrected.
Advisory messages allow you to take a recommended action. This type of message indicates if an operation did not complete or was cancelled.
Informational messages provide instrument status messages. No action is required.
Message Shown on FlexDCA

If the Message Area is not displayed, click Setup > Display Setup to open the Display Setup dialog. Select the Appearance tab and select Dock Message Area.

Messages

Error Messages. Returned over SCPI with :SYSTem:ERRor:NEXT?
Number Message
–XXX A generic message (negative number series) has been reported by the SCPI parser: "this"
–258 Media protected
1 Could not receive from socket
2 Could not send to socket
3 "this" is not a valid choice
10 "this" is at limit
11 "Setting" is set to limit: Entry was out of range
12 "this" entry was not a valid selection
13 "this" is disabled
14 The operation was not completed. The instrument is busy or not responding.
15 "string" entry was limited to "maximum number" characters
16 Invalid character(s) removed from "this" entry
17 ""file name extension" is not a valid extension for "this". Using extension ""default extension"".
18 Invalid file name: "file name"
19 "Setting" must have at least "mimimum number of" values
20 "Setting" cannot have more than "maximum number of" values
30 Unable to read from signal "signal".
31 Unable to write to signal "signal".
40 "this" has recovered from an unexpected software problem.
41 "this" is busy or not responding.
42 Out of memory. Restart the application as soon as possible.
43 Insufficient memory to process "this" . Reduce the record length or turn off some signals.
44 This feature is not supported.
45 Unable to access the clipboard.
46 "application" Restart the application as soon as possible.
47 "Ensure that the application is displayed in the active window before performing a screen capture..
80 Incompatible file: Cannot load "file" into "destination" .
81 Unable to digitally sign exported data: "data type"
82 "this" : "this"
83 Unknown file format or version.
84 Unable to save: reason
85 Unable to load due to insufficient memory.
86 A serious problem has occurred while loading/saving a memory.
87 File is corrupt: "this"
88 The file specifies clock times that are not monotonically increasing.
100 The remote "application/instrument" did not respond.
101 The connection to the remote "application/instrument" has been lost.
102 An unexpected remote "this" communication error occurred: "this"
107 Connected to: "this"
108 Unable to connect: "reason"
110 Waveforms are restricted in length to "length"
120 Unable to write to file "file name"
121 Unable to read from file ""file name" "
122 Could not load ""file name" ": reason
123 Could not find file "file name"
124 Please select a file "file name"
125 File save complete: "file name"
126 Successfully loaded "file name"
127 Preset "preset name" saved successfully.
128 Preset "preset name" loaded successfully.
129 "message"
133 Connection failed: "connection"
134 User driver command error: "driver" returned "reason"
135 User driver initialization timed out
136 User driver command timed out: "driver"
137 User driver command timed out: "driver""
160 Unable to start the "Keysight" or "Pathwave" License Manager.
161 Unable to find the "Keysight" or "Pathwave" License Manager. Verify that it was installed correctly and try again.
162 Connecting to the "Keysight" License Service...
163 Unable to connect to the "Keysight" or "Pathwave" License Service.
165 PathWave License Service Error: "error"
174 The "Interface" SCPI server is running on "port".
175 The "Interface" SCPI server could not be started "port".
176 The "Interface" SCPI server is not running.
181 The "Keysight" License Service is unavailable.
182 The feature "feature name" is unlicensed.
250 Unexpected error in external application description file "this" , line "this" .
251 Unexpected error launching external application "this" .
252 "this" is not a registered external application.
253 The external application description file "this" is incomplete.
299 This BETA version of "this" has expired. Please upgrade to a supported version.
300 Unable to set permissions on ""this" "
301 Could not load Help item ""this" "
430 Module calibration is in progress. Do not remove or insert modules!
431 "this" is unsupported"this" .
432 Optical power correction disabled.
433 Connected to "this" switch: "this"
434 Unable to detect supported switch.
435 Connected to user "this" driver: ""this"
436 This computer does not meet the minimum system requirements for FlexOTO.
450 Internal Error: "this"
451 Test program lines with invalid configuration parameters have been removed.
452 Troubleshooting error: "this"