FlexOTO Programmer's Guide
For sampling oscilloscope products
This programmer's guide documents the remote control of the FlexOTO Optical Test Optimizer application and the FlexOTO Stations applications that FlexOTO launches. To learn general information about FlexOTO including front-panel control, refer to the FlexOTO User's Guide help.
if you_want_success:
Click_here_to_read_FlexOTO_Essentials
Click_here_to_read_Programming_Essentials
Click_here_for_GUI-to-SCPI_map
Click_here_for_Python_examples
else:
start_coding!
Additional Information
FlexOTO's programming syntax conforms to the IEEE 488.2 Standard Digital Interface for Programmable Instrumentation and to the Standard Commands for Programmable Instruments (SCPI). For more detailed information regarding the GPIB, the IEEE 488.2 standard, or the SCPI standard, refer to the following books:
- International Institute of Electrical and Electronics Engineers. IEEE Standard 488.1-1987, IEEE Standard Digital Interface for Programmable Instrumentation. New York, NY, 1987.
- International Institute of Electrical and Electronics Engineers. IEEE Standard 488.2-1987, IEEE Standard Codes, Formats, Protocols and Common commands For Use with ANSI/IEEE Std 488.1-1987. New York, NY, 1987.
When FlexOTO is being remotely controlled, the application displays "Under Remote Control" as shown in the following picture. To return the application from being remotely controlled to front-panel control, either click the displayed Local, shown in this picture, or send the :SYSTem:GTLocal command. After this is done, sending any SCPI command returns FlexOTO to remote mode.