:CALibrate:CANCel
Flex Apps:
FlexDCA
FlexRT
FlexPLL
FlexOTO
Command Syntax
:CALibrate:CANCel
Description
Cancels all calibrations that are in process. During a calibration, message or decision dialogs often appear and this command is equivalent to clicking the dialog's Cancel button. Use the :CALibrate:CONTinue command for an equivalent of the Next button. Use the :CALibrate:SDONe command to pause your application until the user clicks a button and to determine which button was pressed.
Requires FlexPLL revision A.06.70 and above.