Default Setup
On FlexPLL, click Setup > Default Setup to return the FlexPLL to a known start-up state. To set FlexPLL to its factory preset condition, click Setup > Factory Preset. You may find it helpful to use the default settings when initially setting up FlexPLL to view signals or to troubleshoot unexpected instrument behavior. The default settings are listed in the following table.
| Feature | Setting |
|---|---|
| Acquisition | |
| Run/Stop | Run |
| Start Frequency | 1.5 kHz |
| Stop Frequency | 50 MHz |
| Points/Decade | 15 |
| Averaging | Off |
| Number of Averages | 4 |
| Display | |
| UI Color Theme | not changed |
| Dock Message Area | not changed |
| Invert Graph Colors | not changed |
| Source Setup | |
| Remote Source Settings | not changed |
| Jitter Settings | not changed |
| Receiver Setup | |
| Remote DCA Settings | not changed |
| CDR Settings | not changed |
| JTF Graph Setup | |
| Response | On |
| Response Memories | Off |
| Start Frequency | 1.5 kHz |
| Stop Frequency | 50 MHz |
| Center Frequency | 25.00075 MHz |
| Frequency Span | 49.9985 MHz |
| Y-Axis Stop | 10 dB |
| Y-Axis Start | –50 dB |