Factory Preset
Click Setup > Factory Preset to restore FlexPLL to its factory preset settings. Factory preset is the combination of the default settings and the settings listed in the following table.
| Feature | Setting |
|---|---|
| SCPI Server Setup | |
| GPIB | Enabled |
| VXI-11 | Enabled |
| USB | Enabled |
| Telnet | Disabled |
| Sockets | Enabled |
| USB | Enabled |
| Jitter Source Connection Setup Dialog Settings | |
| Connection Method | LAN |
| LAN Server | VXI-11 |
| Host Name / IP Address | HostName |
| VXI-11 Device Index | 0 |
| DCA Connection Setup Dialog Settings | |
| Connection Method | LAN |
| LAN Server | HiSLIP |
| FlexDCA Host Name | HostName |
| HiSLIP1 Device Index | 0 |
| HiSLIP1 Port | 4880 |