Glossary
Typical capacitance parameters of power devices are not always the same as the physical parameters of the device terminal capacitances (Cgd, Cgs, Cds as an example) as shown next. It requires some interpretation to convert them to the data sheet parameters. For example, Ciss is sum of Cgd and Cgs device terminal capacitances.
Power FET Capacitance
IGBT Capacitance
Terms
Cce: Drain to emitter capacitance
Cds: Drain to source capacitance
Cgc: Gate to collector capacitance
Cgd: Gate to drain capacitance
Cge: Gate to emitter capacitance
Cgs: Gate to source capacitance
Cies: IGBT Input capacitance measurement, uses the N1272A.
Ciss: FET Input capacitance measurement. Ciss is sum of Cgd and Cgs device terminal capacitances.
Coes: IGBT Output capacitance, uses the N1272A.
Coss: FET Output capacitance measurement, uses the N1272A.
Cres: IGBT Reverse transfer capacitance measurement, uses the N1272A.
Crss: FET Reverse transfer capacitance, uses the N1272A.
Ic-Vce: For an IGBT, measures Ic-Vce characteristics. SMU pulse is used for the Collector-Emitter voltage output.
Ic-Vge: for an IGBT, measures Ic-Vge characteristics. SMU pulse is used for the Collector-Emitter voltage output.
Ic-Vge for Expander: For an IGBT, measurement uses UHCU, HVMCU and UHVU while the voltage drop at the output resistance of expanders is compensated to make Vce constant.
Ic(off)-Vce: For an IGBT, measures and plots Collector current vs. Collector-Emitter voltage in cutoff region and extracts Collector-Emitter cutoff current and breakdown voltage.
Id-Vds: For FET,
Id-Vgs: For FET,
Id-Vgs for Expander: For FET,
If-Vf: for IGBT and FET,
Ir-Vr: for IGBT and FET,
Rg: For FET, measures gate resistance (in Ohms), uses the N1272A.