PD1000A Power Device Measurement System for Advanced Modeling
Control Software Help includes PD1000A, PD1500A and PD1550A
Welcome
This help file describes the PD1000A Power Device Measurement System for Advanced Modeling control software and how to use it. Specifically, it applies to:
-
PD1000A: Control Software version 2023.324 (or later)
-
PD1500A: Control Software version 2023.324 (or later) with Test Fixture Firmware version A.02.06 (or later) (or later)
-
PD1550A: Control Software version 2023.324 (or later).
The PD1000A graphical user interface main screen contains a task bar, four test selection tabs on the left side, a parameter input area in the center, and a data display area on the right side (for on-state and off-state S-parameter and Double-Pulse tests).
System Summary
The PD1000A Power Device Measurement System for Advanced Modeling consists of several pieces of test equipment plus the PD1000A Control Software. The PD1000A software drives the test measurements, plots the device-under-test measurement data, and saves the measurement data.
An overview of the PD1000A , PD1500A, and the PD1550A systems and how they functions can be found here: System Overview.
Prerequisites
-
Keysight IO Libraries Suite, available free at: www.keysight.com/find/iosuite, is required and must be installed before you can use this control software.
-
Click here for complete system requirements.
-
Download required configuration files for the IV/CV tests. See Install PD1000A Configuration Files for more information.
- S-parameter tests require a PD1010B license
- Double-Pulse Test Measurements require a PD1020A License
- Offline Analysis for Double-Pulse Tests requires a PD1021A license
- GaN device Double-Pulse Tests require a PD1030A license.
- The IV/CV tests do not require licensing.
Getting Started
The PD1000A Control Software has three configuration steps that must be done before running any test:
- Configure Global Settings (see “Settings > Global Settings”) that include the output folder and file names for your characterization data.
- Configure the Test System Hardware for the specific test you want to run.
- Configure the Test System Parameters for the specific test you want to run.
These configuration steps, along with instructions to run a specific test, are described with each system test:
- IV and CV Device Characterization Tests
- S-Parameter Device Characterization Tests
- Double-Pulse Tests (DPT) for Device Characterization (PD1500A)
- Double-Pulse Tests (DPT) for Device Characterization (PD1550A)
Help and Documentation
The
icon opens the PD1000A Help file (the file you are currently reading). While the software is running, you can also open help by pressing the F1 key on the system keyboard. All documentation is available for download at: www.keysight.com/find/PD1000A , www.keysight.com/find/PD1500A, or www.keysight.com/find/PD1550A .
Additional documentation is available in PDF format.
For the PD1000A IV/CV and S-Parameter Device Characterization Test System
- A Startup Guide for setting up the PD1000A hardware IV/CV and ON-State/OFF-State test. Read the Startup Guide to setup and configure the B1505A/B1506A Device Analyzers and the E5080A/B ENA test instruments.
- A Test Fixture Guide.
- A Bias T User Guide
In addition, the IV/CV and S-Parameter tests have an Offline demonstration mode that lets you see what the tests provide. For more information, see:
- IV and CV Offline Mode (formerly Demo Mode)
- On-State and Off-State S-Parameter Offline Mode (formerly Demo Mode)
The Double-Pulse Test (DPT, for PD1500A and PD1550A) software does not have a Offline Mode).
For the PD1500A Double-Pulse Test System:
-
PD1500A Control Software Guide: Provides detailed information to install, configure, and use the PD1000AControl Software for the PD1500ADPT system.
-
PD1500A System Installation Guide: Provides detailed information to install the Double-Pulse Test System Rack and Safety Enclosure at a customer’s site.
-
PD1500A Rack and Safety Enclosure Operation Guide: Provides detailed information to operate and maintain the PD1500ATest Rack and Safety Enclosure.
-
PD1500A Si/Sic Test Fixtures User Guide: Provides detailed information to install and use the Double-Pulse Test Fixture and Test Modules for testing Si/SiC devices in the DPT Test Fixture.
For the PD1550A Double-Pulse Test System:
-
PD1550A Control Software Guide: Provides detailed information to install, configure, and use the PD1000AControl Software for the PD1500ADPT system.
-
PD1550A System Installation Guide: Provides detailed information to install the Double-Pulse Test System Rack and Safety Enclosure at a customer’s site.
-
PD1550A Rack and Safety Enclosure Operation Guide: Provides detailed information to operate and maintain the PD1550ATest Rack and Safety Enclosure.
Contact Keysight
In the United States: 800 829 4844
In Europe: 31 20 547 9999
In Japan: 81 426 56 7832
Use www.keysight.com/find/assist for information on contacting Keysight worldwide or contact your Keysight representative.
See Also
Additional Information About This Product
For additional information, including current data sheets, all PDF manuals, etc., scan a QR code below:
![]()
![]()
![]()
PD1000A Webpage PD1500A Webpage PD1550A Webpage