Output Voltage and Current Peaks

These parameters are not yet implemented but a suggested add-on. It is the output voltage peak during turn-off and output current peak during turn-on. These are important parameters to avoid accidental over-voltage or over-current conditions inside the semiconductor.