IEventIOCompletion::Close

Description

Closes the resource. Sending the resource's COM object's reference count to zero (and thus destroying the object) also executes a close, but this method may be useful for environments with garbage collection or other facilities that make object lifetimes non-deterministic.

VB Prototype

Close(
)

C++ Prototype

HRESULT Close(
);

Return Value

Refer to the table of return codes.

See Also

type, CustomEventTypeNumber, IOStatus, jobId, ReturnCount, ReadBuffer, ReadBufferAsString, GetAttribute, SetAttribute, Close, IEventIOCompletion Overview