IEventIOCompletion::ReadBuffer
Description
The read/written data in the form of a SAFEARRAY of bytes.
VB Prototype
Dim value As SAFEARRAY(BYTE)
value = object.ReadBuffer
C++ Prototype
HRESULT get_ReadBuffer(
SAFEARRAY(BYTE)* ReadBuffer
);
Return Value
Refer to the table of return codes.
See Also
type, CustomEventTypeNumber, IOStatus, jobId, ReturnCount, ReadBuffer, ReadBufferAsString, GetAttribute, SetAttribute, Close, IEventIOCompletion Overview