IEventIOCompletion::IOStatus

Description

The HRESULT of the I/O operation.

VB Prototype

Dim value As HRESULT
value = object.IOStatus

C++ Prototype

HRESULT get_IOStatus(
  HRESULT* IOStatus
);

Return Value

Refer to the table of return codes.

See Also

type, CustomEventTypeNumber, IOStatus, jobId, ReturnCount, ReadBuffer, ReadBufferAsString, GetAttribute, SetAttribute, Close, IEventIOCompletion Overview