IGpib::ProgID
Description
The programmatic ID that can be used by COM to create this object.
VB Prototype
Dim value As String
                                            value = object.ProgID
                                        
C++ Prototype
HRESULT get_ProgID(
                                        
  BSTR* ProgID
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview