IGpib::SoftwareManufacturerID
Description
The ID number of the vendor of this software component.
VB Prototype
Dim value As Short
                                            value = object.SoftwareManufacturerID
                                        
C++ Prototype
HRESULT get_SoftwareManufacturerID(
                                        
  short* SoftwareManufacturerID
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview