IGpib::SecondaryAddress
Description
Secondary address of the GPIB device used by the given session.
VB Prototype
Dim value As Short
                                            value = object.SecondaryAddress
                                        
C++ Prototype
HRESULT get_SecondaryAddress(
                                        
  short* SecondaryAddress
);
		
Return Value
Refer to the table of return codes.
See Also
ComponentVersion, SpecVersion, HardwareInterfaceName, HardwareInterfaceNumber, HardwareInterfaceType, LockState, OptionString, ProgID, ResourceName, SessionType, SoftwareManufacturerID, SoftwareManufacturerName, Timeout, LastStatus, PrimaryAddress, RENState, RepeatAddressingEnabled, SecondaryAddress, UnaddressingEnabled, GetAttribute, SetAttribute, LockRsrc, UnlockRsrc, Init, Close, ControlREN, IGpib Overview